48 #if defined(__cplusplus)
55 #define Mx_S_SUCCESS (0)
60 #define Mx_E_FAIL (-1)
91 int32_t
Mx_add(int32_t a, int32_t b);
93 #if defined(IPC_BUILDOS_QNX)
112 #if defined(__cplusplus)
uint32_t coef
Definition: Mx.h:66
uint32_t * outBuf
Definition: Mx.h:70
Compute structure.
Definition: Mx.h:65
int32_t Mx_compute_Linux(Mx_Compute *compute, int fd, int fdIn, int fdOut)
Sample function which has pointer parameter (DMA_BUF) to a structure with two embedded pointers...
void Mx_finalize(void)
Finalize the module, must be called last.
int key
Definition: Mx.h:67
int Mx_initialize(UInt16 procId)
Initialize the module, must be called first.
int32_t Mx_triple(uint32_t a)
Sample function which multiplies argument by three.
int32_t Mx_add(int32_t a, int32_t b)
Sample function which addes two arguments.
uint32_t * inBuf
Definition: Mx.h:69
int size
Definition: Mx.h:68