![]() |
![]() |
IPC API
3.35.01.07
|
Factory virtual function table. More...
#include <Ipc.h>
Data Fields | |
Int(* | createFxn )(Void) |
Void(* | deleteFxn )(Void) |
Factory virtual function table.
This virtual function table defines the interface which must be implemented by the transport factory. The Ipc module will use this factory to create and delete this transport. The factory is responsible for managing the details of creation and deletion.
Int(* Ipc_TransportFactoryFxns::createFxn)(Void) |
factory create method
Void(* Ipc_TransportFactoryFxns::deleteFxn)(Void) |
factory finalize method