![]() |
![]() |
IPC API
3.30.03.14
|
Function descriptor. More...
#include <RcmServer.h>
Data Fields | |
String | name |
The name of the function. More... | |
RcmServer_MsgFxn | addr |
The function address in the server's address space. More... | |
Function descriptor.
INTERNAL
This function descriptor is used internally in the server. Its values are defined either at config time by the server's RcmServer_Params.fxns create parameter or at runtime through a call to RcmClient_addSymbol().
String RcmServer_FxnDesc::name |
The name of the function.
The name is used for table lookup, it does not search the actual symbol table. You can provide any string as long as it is unique and the client uses the same name for lookup.
RcmServer_MsgFxn RcmServer_FxnDesc::addr |
The function address in the server's address space.
The server will ultimately branch to this address.