Opaque client structure large enough to hold an instance object.
More...
#include <RcmClient.h>
Opaque client structure large enough to hold an instance object.
Use this structure to define an embedded RcmClient object.
- See Also
- RcmClient_construct
xdc_runtime_knl_GateThread_Struct RcmClient_Struct::_f1 |
Ptr RcmClient_Struct::_f2 |
Ptr RcmClient_Struct::_f3 |
UInt16 RcmClient_Struct::_f4 |
Ptr RcmClient_Struct::_f5 |
UInt32 RcmClient_Struct::_f6 |
Bool RcmClient_Struct::_f7 |
UInt16 RcmClient_Struct::_f8 |
Ptr RcmClient_Struct::_f9 |
Ptr RcmClient_Struct::_f10 |
Ptr RcmClient_Struct::_f11 |
Ptr RcmClient_Struct::_f12 |
The documentation for this struct was generated from the following file: