![]() |
![]() |
IPC API
3.22.00.05
|
Structure defining parameters for the GateMP module. More...
#include <GateMP.h>
Data Fields | |
String | name |
UInt16 | regionId |
GateMP_LocalProtect | localProtect |
GateMP_RemoteProtect | remoteProtect |
Structure defining parameters for the GateMP module.
String GateMP_Params::name |
Name of this instance.
The name (if not NULL) must be unique among all GateMP instances in the entire system. The name does not have to be in persistent memory. The supplied string is copied into persistent memory. If no name is supplied, the instance cannot be opened calling GateMP_open(). The max length of the name is defined by the maxNameLen of the NameServer instance.
UInt16 GateMP_Params::regionId |
Shared region ID
The index corresponding to the shared region from which shared memory is allocated for the instance. If not specified, the default of '0' is used, otherwise the specified SharedRegion is used. The amount of shared memory allocated can be determined by calling GateMP_sharedMemReq().
GateMP_LocalProtect GateMP_Params::localProtect |
Local protection level
The default value is GateMP_LocalProtect_THREAD
GateMP_RemoteProtect GateMP_Params::remoteProtect |
Remote protection level
The default value is GateMP_RemoteProtect_SYSTEM