module ti.sdo.utils.MultiProc |
|
|
|
Processor Id Module Manager
Many IPC modules require identifying processors in a
multi-processor environment. The MultiProc module centralizes
processor id management into one module. Since this configuration
is almost always universally required, most IPC applications
require supplying configuration of this module.
[
more ... ]
#include <ti/sdo/utils/MultiProc.h>
Functions common to all target modules |
|
|
Defines |
#define | |
Constants |
| |
| |
extern const UInt16 | |
DETAILS
Many IPC modules require identifying processors in a
multi-processor environment. The MultiProc module centralizes
processor id management into one module. Since this configuration
is almost always universally required, most IPC applications
require supplying configuration of this module.
Each processor in the MultiProc module may be uniquely identified by
either a name string or an integer ranging from 0 to MAXPROCESSORS - 1.
Configuration is supplied using the
setConfig meta function,
the
numProcessors and
baseIdOfCluster.
The setConfig function tells the MultiProc module:
- The specific processor for which the application is being built
- The number of processors in the cluster
A cluster is a set of processors within a system which share some share
shared memory and supports notifications. Typically most systems contain
one cluster. When there are multiple clusters in the system, the
numProcessors and
baseIdOfCluster configuration
paramaters are required to be set before calling
setConfig
For examle in a system with 2 C6678 devices [each C6678 contains 8
homogeneuous cores]. For first C6678 device:
var MultiProc = xdc.useModule('ti.sdo.utils.MultiProc');
MultiProc.baseIdOfCluster = 0;
MultiProc.numProcessors = 16;
MultiProc.setConfig(null, ["CORE0", "CORE1", "CORE2", "CORE3",
"CORE4", "CORE5", "CORE6", "CORE7"]);
For second C6678 device:
var MultiProc = xdc.useModule('ti.sdo.utils.MultiProc');
MultiProc.baseIdOfCluster = 8;
MultiProc.numProcessors = 16;
MultiProc.setConfig(null, ["CORE0", "CORE1", "CORE2", "CORE3",
"CORE4", "CORE5", "CORE6", "CORE7"]);
Using the information supplied using the
setConfig meta function
and the
baseIdOfCluster module configuration, the processor IDs
are internally set. Please refer to the documentation for
setConfig and
baseIdOfCluster for more details.
At runtime, the
getId call returns the MultiProc id of those
processors within its cluster. At config-time, the
getIdMeta
call returns the the same value.
const MultiProc_INVALIDID |
|
Invalid processor id constant
#define MultiProc_INVALIDID (UInt16)0xFFFF
DETAILS
This constant denotes that the processor id is not valid.
config MultiProc_A_invalidMultiProcId // module-wide |
|
Assert raised when an invalid processor id is used
extern const Assert_Id MultiProc_A_invalidMultiProcId;
config MultiProc_A_invalidProcName // module-wide |
|
Assert raised when a NULL processor name is encountered
extern const Assert_Id MultiProc_A_invalidProcName;
config MultiProc_numProcessors // module-wide |
|
Number of processors in the system
extern const UInt16 MultiProc_numProcessors;
DETAILS
This configuration should only be set when there is more than one
cluster in the system. It must be set before calling
setConfig. If the system contains only one cluster,
it is internally set by the
setConfig meta function to the
length of the supplied nameList array.
After
setConfig has been called, it is possible to
retrive the maximum # of processors by reading this module config
either at run-time or at config time.
Module-Wide Built-Ins |
|
// Get this module's unique id
Bool MultiProc_Module_startupDone();
// Test if this module has completed startup
// The heap from which this module allocates memory
Bool MultiProc_Module_hasMask();
// Test whether this module has a diagnostics mask
Bits16 MultiProc_Module_getMask();
// Returns the diagnostics mask for this module
Void MultiProc_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
var MultiProc = xdc.useModule('ti.sdo.utils.MultiProc');
module-wide constants & types
module-wide config parameters
msg: "A_invalidMultiProcId: Invalid MultiProc id"
};
msg: "A_invalidProcName: NULL MultiProc name encountered"
};
module-wide functions
const MultiProc.INVALIDID |
|
Invalid processor id constant
XDCscript usage |
meta-domain |
const MultiProc.INVALIDID = 0xFFFF;
DETAILS
This constant denotes that the processor id is not valid.
C SYNOPSIS
metaonly struct MultiProc.ModuleView |
|
XDCscript usage |
meta-domain |
var obj = new MultiProc.ModuleView;
obj.id = UInt16 ...
obj.numProcessors = UInt16 ...
obj.nameList = String[] ...
config MultiProc.A_invalidMultiProcId // module-wide |
|
Assert raised when an invalid processor id is used
XDCscript usage |
meta-domain |
msg: "A_invalidMultiProcId: Invalid MultiProc id"
};
C SYNOPSIS
config MultiProc.A_invalidProcName // module-wide |
|
Assert raised when a NULL processor name is encountered
XDCscript usage |
meta-domain |
msg: "A_invalidProcName: NULL MultiProc name encountered"
};
C SYNOPSIS
config MultiProc.numProcessors // module-wide |
|
Number of processors in the system
XDCscript usage |
meta-domain |
MultiProc.numProcessors = UInt16 1;
DETAILS
This configuration should only be set when there is more than one
cluster in the system. It must be set before calling
setConfig. If the system contains only one cluster,
it is internally set by the
setConfig meta function to the
length of the supplied nameList array.
After
setConfig has been called, it is possible to
retrive the maximum # of processors by reading this module config
either at run-time or at config time.
C SYNOPSIS
metaonly config MultiProc.baseIdOfCluster // module-wide |
|
The base id of the cluster
XDCscript usage |
meta-domain |
MultiProc.baseIdOfCluster = UInt16 0;
DETAILS
Using this base id, the id of each processor in the cluster
is set based up its position in
setConfig. When more
more than one cluster exists in the system, this parameter must
be set before calling
setConfig.
metaonly config MultiProc.common$ // module-wide |
|
Common module configuration parameters
XDCscript usage |
meta-domain |
DETAILS
All modules have this configuration parameter. Its name
contains the '$' character to ensure it does not conflict with
configuration parameters declared by the module. This allows
new configuration parameters to be added in the future without
any chance of breaking existing modules.
metaonly config MultiProc.rovViewInfo // module-wide |
|
XDCscript usage |
meta-domain |
metaonly MultiProc.getDeviceProcNames() // module-wide |
|
Returns an array of all possible processor names on the build device
XDCscript usage |
meta-domain |
MultiProc.getDeviceProcNames() returns Any
DETAILS
@(return) Array of valid MultiProc processor names
metaonly MultiProc.getIdMeta() // module-wide |
|
Meta version of getId
XDCscript usage |
meta-domain |
MultiProc.getIdMeta(String name) returns UInt16
ARGUMENTS
name
MultiProc procName
DETAILS
Statically returns the internally set ID based on configuration
supplied via
setConfig.
metaonly MultiProc.setConfig() // module-wide |
|
Configure the MultiProc module
XDCscript usage |
meta-domain |
MultiProc.setConfig(String name, String[] nameList) returns Void
ARGUMENTS
name
MultiProc name for the local processor
nameList
Array of all processors used by the application
DETAILS
Configuration of the MultiProc module is primarily accomplished using
the setConfig API at config time. The setConfig API allows the
MultiProc module to identify:
- Which is the local processor
- Which processors are being used
- Which processors can synchronize
The second of these two pieces of information is supplied via the
nameList argument. The nameList is a non-empty set of distinct
processors valid for the particular device. For a list of valid
processor names for a given device, please refer to the :
Table of
Valid Names for Each Device.
The local processor is identified by using a single name from
nameList. A MultiProc id is internally set to the index of
'name' in the supplied 'nameList'. I.e. in the example:
MultiProc.setConfig("DSP", ["HOST", "DSP", "OTHERCORE"]);
The processors, "HOST", "DSP" and "OTHERCORE" get assigned MultiProc
IDs 0, 1, and 2, respectively. The local processor, "DSP" is assigned
an ID of '1'.
If the local processor is not known at static time, it is possible to
supply a null name. MultiProc will set the local id to
INVALIDID until it is set at runtime using
MultiProc_setLocalId.
generated on Fri, 10 May 2013 19:39:31 GMT