Project  1.0
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Pages
Data Fields
HeapBufMP_Params Struct Reference

Structure defining parameters for the HeapBufMP module. More...

#include <HeapBufMP.h>

Data Fields

String name
UInt16 regionId
SizeT blockSize
UInt numBlocks
SizeT align
Bool exact
GateMP_Handle gate

Detailed Description

Structure defining parameters for the HeapBufMP module.


Field Documentation

String HeapBufMP_Params::name

Name of this instance.

   The name (if not NULL) must be unique among all HeapBufMP
   instances in the entire system.  When creating a new
   heap, it is necessary to supply an instance name.

   The name does not have to be persistent.  The supplied string is copied
   into persistent memory.
UInt16 HeapBufMP_Params::regionId

Shared region ID

   The index corresponding to the shared region from which shared memory
   will be allocated.
SizeT HeapBufMP_Params::blockSize

Size (in MAUs) of each block.

HeapBufMP will round the blockSize up to the nearest multiple of the alignment, so the actual blockSize may be larger. When creating a HeapBufMP dynamically, this needs to be taken into account to determine the proper buffer size to pass in.

Required parameter.

The default size of the blocks is 0 MAUs.

UInt HeapBufMP_Params::numBlocks

Number of fixed-size blocks.

    This is a required parameter for all new HeapBufMP instances.
SizeT HeapBufMP_Params::align

Alignment (in MAUs) of each block.

   The alignment must be a power of 2. If the value 0 is specified,
   the value will be changed to meet minimum structure alignment 
   requirements and the cache alignment size of the region in which the
   heap will be placed.  Therefore, the actual alignment may be larger.

   The default alignment is 0.
Bool HeapBufMP_Params::exact

Use exact matching

   Setting this flag will allow allocation only if the requested size
   is equal to (rather than less than or equal to) the buffer's block
   size.
GateMP_Handle HeapBufMP_Params::gate

GateMP used for critical region management of the shared memory

   Using the default value of NULL will result in use of the GateMP
   system gate for context protection.

The documentation for this struct was generated from the following file:
Copyright 2013, Texas Instruments Incorporated