Project
1.0
|
Stats structure for the HeapBufMP_getExtendedStats API. More...
#include <HeapBufMP.h>
Data Fields | |
UInt | maxAllocatedBlocks |
UInt | numAllocatedBlocks |
Stats structure for the HeapBufMP_getExtendedStats API.
UInt HeapBufMP_ExtendedStats::maxAllocatedBlocks |
The maximum number of blocks allocated from this heap at any point in time during the lifetime of this HeapBufMP instance.
UInt HeapBufMP_ExtendedStats::numAllocatedBlocks |
The total number of blocks currently allocated in this HeapBufMP instance.