module ti.sdo.ipc.family.dm6446.InterruptArm

DM6446 based interrupt manager

C synopsis target-domain sourced in ti/sdo/ipc/family/dm6446/InterruptArm.xdc
 
struct InterruptArm_IntInfo
C synopsis target-domain
typedef struct InterruptArm_IntInfo {
    UInt localIntId;
    UInt remoteIntId;
    UInt intVectorId;
} InterruptArm_IntInfo;
 
 
InterruptArm_intClear()  // module-wide

Clear interrupt

C synopsis target-domain
UInt InterruptArm_intClear(UInt16 remoteProcId, IInterrupt_IntInfo *intInfo);
 
ARGUMENTS
remoteProcId — Remote MultiProc Id
intInfo — Information needed to configure interrupt line
RETURNS
Value (if any) of the interrupt before it was cleared
 
InterruptArm_intDisable()  // module-wide

Disables the interrupt corresponding to intId

C synopsis target-domain
Void InterruptArm_intDisable(UInt16 remoteProcId, IInterrupt_IntInfo *intInfo);
 
ARGUMENTS
remoteProcId — Remote MultiProc Id
intInfo — Information needed to configure interrupt line
 
InterruptArm_intEnable()  // module-wide

Enables the interrupt corresponding to intId

C synopsis target-domain
Void InterruptArm_intEnable(UInt16 remoteProcId, IInterrupt_IntInfo *intInfo);
 
ARGUMENTS
remoteProcId — Remote MultiProc Id
intInfo — Information needed to configure interrupt line
 
InterruptArm_intRegister()  // module-wide

Register an interrupt line to a remote processor

C synopsis target-domain
Void InterruptArm_intRegister(UInt16 remoteProcId, IInterrupt_IntInfo *intInfo, Fxn func, UArg arg);
 
ARGUMENTS
remoteProcId — Remote MultiProc Id
intInfo — Information needed to configure interrupt line
func — Function to register.
arg — Argument that will be passed to func
 
InterruptArm_intSend()  // module-wide

Send interrupt to the remote processor

C synopsis target-domain
Void InterruptArm_intSend(UInt16 remoteProcId, IInterrupt_IntInfo *intInfo, UArg arg);
 
ARGUMENTS
remoteProcId — Remote MultiProc Id
intInfo — Information needed to configure interrupt line
arg — Argument for sending interrupt.
 
InterruptArm_intUnregister()  // module-wide

Unregister an interrupt line to a remote processor

C synopsis target-domain
Void InterruptArm_intUnregister(UInt16 remoteProcId, IInterrupt_IntInfo *intInfo);
 
ARGUMENTS
remoteProcId — Remote MultiProc Id
intInfo — Information needed to configure interrupt line
Module-Wide Built-Ins

C synopsis target-domain
Types_ModuleId InterruptArm_Module_id();
// Get this module's unique id
 
Bool InterruptArm_Module_startupDone();
// Test if this module has completed startup
 
IHeap_Handle InterruptArm_Module_heap();
// The heap from which this module allocates memory
 
Bool InterruptArm_Module_hasMask();
// Test whether this module has a diagnostics mask
 
Bits16 InterruptArm_Module_getMask();
// Returns the diagnostics mask for this module
 
Void InterruptArm_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
 
XDCscript usage meta-domain sourced in ti/sdo/ipc/family/dm6446/InterruptArm.xdc
var InterruptArm = xdc.useModule('ti.sdo.ipc.family.dm6446.InterruptArm');
module-wide constants & types
    var obj = new InterruptArm.IntInfo// ;
        obj.localIntId = UInt  ...
        obj.remoteIntId = UInt  ...
        obj.intVectorId = UInt  ...
module-wide config parameters
 
 
struct InterruptArm.IntInfo
XDCscript usage meta-domain
var obj = new InterruptArm.IntInfo;
 
    obj.localIntId = UInt  ...
    obj.remoteIntId = UInt  ...
    obj.intVectorId = UInt  ...
 
C SYNOPSIS
 
metaonly config InterruptArm.common$  // module-wide

Common module configuration parameters

XDCscript usage meta-domain
InterruptArm.common$ = Types.Common$ undefined;
 
DETAILS
All modules have this configuration parameter. Its name contains the '$' character to ensure it does not conflict with configuration parameters declared by the module. This allows new configuration parameters to be added in the future without any chance of breaking existing modules.
generated on Tue, 22 May 2012 23:44:42 GMT