module ti.sdo.utils.NameServerRemoteNull
C synopsis target-domain sourced in ti/sdo/utils/NameServerRemoteNull.xdc
#include <ti/sdo/utils/NameServerRemoteNull.h>
Functions
Void
Void
Void
Void
Functions common to all INameServerRemote modules
Int 
Int 
Int 
NameServerRemoteNull_get// (NameServerRemoteNull_Handle handle, String instanceName, String name, Ptr value, UInt32 *valueLen, ISync_Handle syncHandle, Error_Block *eb);
SizeT 
Functions common to all target instances
Functions common to all target modules
Typedefs
typedef struct
typedef struct
typedef enum
typedef struct
 
 
enum NameServerRemoteNull_Status

Status codes returned by certain calls

C synopsis target-domain
typedef enum NameServerRemoteNull_Status {
    NameServerRemoteNull_S_SUCCESS,
    NameServerRemoteNull_E_FAIL,
    NameServerRemoteNull_E_ERROR
} NameServerRemoteNull_Status;
 
 
NameServerRemoteNull_attach()  // module-wide

Function is called by Ipc_attach() through NameServer_SetupProxy

C synopsis target-domain
Int NameServerRemoteNull_attach(UInt16 remoteProcId, Ptr sharedAddr);
 
 
NameServerRemoteNull_detach()  // module-wide

Function is called by Ipc_detach() through NameServer_SetupProxy

C synopsis target-domain
Int NameServerRemoteNull_detach(UInt16 remoteProcId);
 
 
NameServerRemoteNull_sharedMemReq()  // module-wide

Returns the shared memory size requirement for a single instance

C synopsis target-domain
SizeT NameServerRemoteNull_sharedMemReq(Ptr sharedAddr);
 
ARGUMENTS
sharedAddr — Shared address
RETURNS
Number of MAUs needed to create the instance.
DETAILS
Function is called during Ipc_attach() through NameServer_SetupProxy.
Module-Wide Built-Ins

C synopsis target-domain
Types_ModuleId NameServerRemoteNull_Module_id();
// Get this module's unique id
 
Bool NameServerRemoteNull_Module_startupDone();
// Test if this module has completed startup
 
IHeap_Handle NameServerRemoteNull_Module_heap();
// The heap from which this module allocates memory
 
Bool NameServerRemoteNull_Module_hasMask();
// Test whether this module has a diagnostics mask
 
Bits16 NameServerRemoteNull_Module_getMask();
// Returns the diagnostics mask for this module
 
Void NameServerRemoteNull_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
Instance Object Types

C synopsis target-domain
typedef struct NameServerRemoteNull_Object NameServerRemoteNull_Object;
// Opaque internal representation of an instance object
 
typedef NameServerRemoteNull_Object *NameServerRemoteNull_Handle;
// Client reference to an instance object
 
typedef struct NameServerRemoteNull_Struct NameServerRemoteNull_Struct;
// Opaque client structure large enough to hold an instance object
 
NameServerRemoteNull_Handle NameServerRemoteNull_handle(NameServerRemoteNull_Struct *structP);
// Convert this instance structure pointer into an instance handle
 
NameServerRemoteNull_Struct *NameServerRemoteNull_struct(NameServerRemoteNull_Handle handle);
// Convert this instance handle into an instance structure pointer
Instance Config Parameters

C synopsis target-domain
typedef struct NameServerRemoteNull_Params {
// Instance config-params structure
    IInstance_Params *instance;
    // Common per-instance configs
} NameServerRemoteNull_Params;
 
Void NameServerRemoteNull_Params_init(NameServerRemoteNull_Params *params);
// Initialize this config-params structure with supplier-specified defaults before instance creation
Instance Creation

C synopsis target-domain
NameServerRemoteNull_Handle NameServerRemoteNull_create(UInt16 procId, const NameServerRemoteNull_Params *params, Error_Block *eb);
// Allocate and initialize a new instance object and return its handle
 
Void NameServerRemoteNull_construct(NameServerRemoteNull_Struct *structP, UInt16 procId, const NameServerRemoteNull_Params *params);
// Initialize a new instance object inside the provided structure
ARGUMENTS
params — per-instance config params, or NULL to select default values (target-domain only)
eb — active error-handling block, or NULL to select default policy (target-domain only)
Instance Deletion

C synopsis target-domain
Void NameServerRemoteNull_delete(NameServerRemoteNull_Handle *handleP);
// Finalize and free this previously allocated instance object, setting the referenced handle to NULL
 
Void NameServerRemoteNull_destruct(NameServerRemoteNull_Struct *structP);
// Finalize the instance object inside the provided structure
 
NameServerRemoteNull_get()  // instance
C synopsis target-domain
Int NameServerRemoteNull_get(NameServerRemoteNull_Handle handle, String instanceName, String name, Ptr value, UInt32 *valueLen, ISync_Handle syncHandle, Error_Block *eb);
 
ARGUMENTS
handle — handle of a previously-created NameServerRemoteNull instance object
Instance Convertors

C synopsis target-domain
INameServerRemote_Handle NameServerRemoteNull_Handle_upCast(NameServerRemoteNull_Handle handle);
// unconditionally move one level up the inheritance hierarchy
 
NameServerRemoteNull_Handle NameServerRemoteNull_Handle_downCast(INameServerRemote_Handle handle);
// conditionally move one level down the inheritance hierarchy; NULL upon failure
Instance Built-Ins

C synopsis target-domain
Int NameServerRemoteNull_Object_count();
// The number of statically-created instance objects
 
NameServerRemoteNull_Handle NameServerRemoteNull_Object_get(NameServerRemoteNull_Object *array, Int i);
// The handle of the i-th statically-created instance object (array == NULL)
 
NameServerRemoteNull_Handle NameServerRemoteNull_Object_first();
// The handle of the first dynamically-created instance object, or NULL
 
NameServerRemoteNull_Handle NameServerRemoteNull_Object_next(NameServerRemoteNull_Handle handle);
// The handle of the next dynamically-created instance object, or NULL
 
IHeap_Handle NameServerRemoteNull_Object_heap();
// The heap used to allocate dynamically-created instance objects
 
Types_Label *NameServerRemoteNull_Handle_label(NameServerRemoteNull_Handle handle, Types_Label *buf);
// The label associated with this instance object
 
String NameServerRemoteNull_Handle_name(NameServerRemoteNull_Handle handle);
// The name of this instance object
 
XDCscript usage meta-domain sourced in ti/sdo/utils/NameServerRemoteNull.xdc
var NameServerRemoteNull = xdc.useModule('ti.sdo.utils.NameServerRemoteNull');
module-wide constants & types
        const NameServerRemoteNull.S_SUCCESS;
        const NameServerRemoteNull.E_FAIL;
        const NameServerRemoteNull.E_ERROR;
module-wide config parameters
per-instance config parameters
    var params = new NameServerRemoteNull.Params// Instance config-params object;
per-instance creation
    var inst = NameServerRemoteNull.create// Create an instance-object(UInt16 procId, params);
 
 
enum NameServerRemoteNull.Status

Status codes returned by certain calls

XDCscript usage meta-domain
values of type NameServerRemoteNull.Status
    const NameServerRemoteNull.S_SUCCESS;
    const NameServerRemoteNull.E_FAIL;
    const NameServerRemoteNull.E_ERROR;
 
C SYNOPSIS
 
metaonly config NameServerRemoteNull.common$  // module-wide

Common module configuration parameters

XDCscript usage meta-domain
NameServerRemoteNull.common$ = Types.Common$ undefined;
 
DETAILS
All modules have this configuration parameter. Its name contains the '$' character to ensure it does not conflict with configuration parameters declared by the module. This allows new configuration parameters to be added in the future without any chance of breaking existing modules.
Instance Config Parameters

XDCscript usage meta-domain
var params = new NameServerRemoteNull.Params;
// Instance config-params object
Instance Creation

XDCscript usage meta-domain
var params = new NameServerRemoteNull.Params;
// Allocate instance config-params
params.config =   ...
// Assign individual configs
 
var inst = NameServerRemoteNull.create(UInt16 procId, params);
// Create an instance-object
ARGUMENTS
params — per-instance config params, or NULL to select default values (target-domain only)
eb — active error-handling block, or NULL to select default policy (target-domain only)
generated on Sat, 11 Feb 2012 00:38:14 GMT