const GateHWSpinlock_Q_BLOCKING |
|
Blocking quality
#define GateHWSpinlock_Q_BLOCKING (Int)1
DETAILS
Gates with this "quality" may cause the calling thread to block;
i.e., suspend execution until another thread leaves the gate.
const GateHWSpinlock_Q_PREEMPTING |
|
Preempting quality
#define GateHWSpinlock_Q_PREEMPTING (Int)2
DETAILS
Gates with this "quality" allow other threads to preempt the thread
that has already entered the gate.
config GateHWSpinlock_A_invSpinLockNum // module-wide |
|
Assert raised when provided lockNum is invalid for the relevant device
extern const Assert_Id GateHWSpinlock_A_invSpinLockNum;
config GateHWSpinlock_LM_close // module-wide |
|
Logged on gate close
extern const Log_Event GateHWSpinlock_LM_close;
config GateHWSpinlock_LM_create // module-wide |
|
Logged on gate create
extern const Log_Event GateHWSpinlock_LM_create;
config GateHWSpinlock_LM_delete // module-wide |
|
Logged on gate deletion
extern const Log_Event GateHWSpinlock_LM_delete;
config GateHWSpinlock_LM_enter // module-wide |
|
Logged on gate enter
extern const Log_Event GateHWSpinlock_LM_enter;
config GateHWSpinlock_LM_leave // module-wide |
|
Logged on gate leave
extern const Log_Event GateHWSpinlock_LM_leave;
config GateHWSpinlock_LM_open // module-wide |
|
Logged on gate open
extern const Log_Event GateHWSpinlock_LM_open;
config GateHWSpinlock_baseAddr // module-wide |
|
Device-specific base address for HW Semaphore subsystem
extern const Ptr GateHWSpinlock_baseAddr;
GateHWSpinlock_query() // module-wide |
|
Runtime test for a particular gate quality
Bool GateHWSpinlock_query(Int qual);
ARGUMENTS
qual
constant describing a quality
RETURNS
Returns TRUE if the gate has the given quality,
and FALSE otherwise, which includes the case when the gate does not
recognize the constant describing the quality.
GateHWSpinlock_sharedMemReq() // module-wide |
|
Amount of shared memory required for creation of each instance
ARGUMENTS
params
Pointer to the parameters that will be used in
the create.
DETAILS
The value returned by this function may depend on the cache alignment
requirements for the shared region from which memory will be used.
RETURNS
Number of MAUs needed to create the instance.
Module-Wide Built-Ins |
|
// Get this module's unique id
Bool GateHWSpinlock_Module_startupDone();
// Test if this module has completed startup
// The heap from which this module allocates memory
Bool GateHWSpinlock_Module_hasMask();
// Test whether this module has a diagnostics mask
Bits16 GateHWSpinlock_Module_getMask();
// Returns the diagnostics mask for this module
Void GateHWSpinlock_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
Instance Object Types |
|
typedef struct GateHWSpinlock_Object GateHWSpinlock_Object;
// Opaque internal representation of an instance object
// Client reference to an instance object
typedef struct GateHWSpinlock_Struct GateHWSpinlock_Struct;
// Opaque client structure large enough to hold an instance object
// Convert this instance structure pointer into an instance handle
// Convert this instance handle into an instance structure pointer
Instance Config Parameters |
|
typedef struct GateHWSpinlock_Params {
// Instance config-params structure
// Common per-instance configs
UInt resourceId;
// Logical resource id
Ptr sharedAddr;
// Physical address of the shared memory
} GateHWSpinlock_Params;
// Initialize this config-params structure with supplier-specified defaults before instance creation
config GateHWSpinlock_resourceId // instance |
|
Logical resource id
config GateHWSpinlock_sharedAddr // instance |
|
Physical address of the shared memory
DETAILS
This parameter is only used by GateMP delegates that use shared memory
Instance Creation |
|
// Allocate and initialize a new instance object and return its handle
// Initialize a new instance object inside the provided structure
ARGUMENTS
localGate
Gate to use for local protection.
params
per-instance config params, or NULL to select default values (target-domain only)
eb
active error-handling block, or NULL to select default policy (target-domain only)
DETAILS
A Non-NULL gate for local protection must be passed to the create
call. If no local protection is desired, a
xdc.runtime.GateNull handle must be passed in.
Instance Deletion |
|
// Finalize and free this previously allocated instance object, setting the referenced handle to NULL
// Finalize the instance object inside the provided structure
Instance Convertors |
|
// unconditionally move one level up the inheritance hierarchy
// conditionally move one level down the inheritance hierarchy; NULL upon failure
// unconditionally move 2 levels up the inheritance hierarchy
// conditionally move 2 levels down the inheritance hierarchy; NULL upon failure
Instance Built-Ins |
|
Int GateHWSpinlock_Object_count();
// The number of statically-created instance objects
// The handle of the i-th statically-created instance object (array == NULL)
// The handle of the first dynamically-created instance object, or NULL
// The handle of the next dynamically-created instance object, or NULL
// The heap used to allocate dynamically-created instance objects
// The label associated with this instance object
// The name of this instance object
const GateHWSpinlock.Q_BLOCKING |
|
Blocking quality
XDCscript usage |
meta-domain |
const GateHWSpinlock.Q_BLOCKING = 1;
DETAILS
Gates with this "quality" may cause the calling thread to block;
i.e., suspend execution until another thread leaves the gate.
C SYNOPSIS
const GateHWSpinlock.Q_PREEMPTING |
|
Preempting quality
XDCscript usage |
meta-domain |
const GateHWSpinlock.Q_PREEMPTING = 2;
DETAILS
Gates with this "quality" allow other threads to preempt the thread
that has already entered the gate.
C SYNOPSIS
config GateHWSpinlock.A_invSpinLockNum // module-wide |
|
Assert raised when provided lockNum is invalid for the relevant device
XDCscript usage |
meta-domain |
msg: "A_invSpinLockNum: Invalid hardware spinlock number"
};
C SYNOPSIS
config GateHWSpinlock.LM_close // module-wide |
|
Logged on gate close
XDCscript usage |
meta-domain |
msg: "LM_close: Gate (lockNum = %d) closed"
};
C SYNOPSIS
config GateHWSpinlock.LM_create // module-wide |
|
Logged on gate create
XDCscript usage |
meta-domain |
msg: "LM_create: Gate (lockNum = %d) created"
};
C SYNOPSIS
config GateHWSpinlock.LM_delete // module-wide |
|
Logged on gate deletion
XDCscript usage |
meta-domain |
msg: "LM_delete: Gate (lockNum = %d) deleted"
};
C SYNOPSIS
config GateHWSpinlock.LM_enter // module-wide |
|
Logged on gate enter
XDCscript usage |
meta-domain |
msg: "LM_enter: Gate (lockNum = %d) entered, returning key = %d"
};
C SYNOPSIS
config GateHWSpinlock.LM_leave // module-wide |
|
Logged on gate leave
XDCscript usage |
meta-domain |
msg: "LM_leave: Gate (lockNum = %d) left using key = %d"
};
C SYNOPSIS
config GateHWSpinlock.LM_open // module-wide |
|
Logged on gate open
XDCscript usage |
meta-domain |
msg: "LM_open: Remote gate (lockNum = %d) opened"
};
C SYNOPSIS
config GateHWSpinlock.baseAddr // module-wide |
|
Device-specific base address for HW Semaphore subsystem
XDCscript usage |
meta-domain |
GateHWSpinlock.baseAddr = Ptr null;
C SYNOPSIS
metaonly config GateHWSpinlock.common$ // module-wide |
|
Common module configuration parameters
XDCscript usage |
meta-domain |
DETAILS
All modules have this configuration parameter. Its name
contains the '$' character to ensure it does not conflict with
configuration parameters declared by the module. This allows
new configuration parameters to be added in the future without
any chance of breaking existing modules.
metaonly GateHWSpinlock.getNumResources() // module-wide |
|
Returns the number of resources offered by the GateMP delegate
XDCscript usage |
meta-domain |
GateHWSpinlock.getNumResources() returns UInt
metaonly GateHWSpinlock.queryMeta() // module-wide |
|
Configuration time test for a particular gate quality
XDCscript usage |
meta-domain |
GateHWSpinlock.queryMeta(Int qual) returns Bool
ARGUMENTS
qual
constant describing a quality
RETURNS
Returns TRUE if the gate has the given quality,
and FALSE otherwise, which includes the case when the gate does not
recognize the constant describing the quality.
metaonly GateHWSpinlock.setReserved() // module-wide |
|
Reserve a HW spinlock for use outside of IPC
XDCscript usage |
meta-domain |
GateHWSpinlock.setReserved(UInt lockNum) returns Void
ARGUMENTS
lockNum
HW spinlock number to reserve
DETAILS
GateMP will, by default, manage all HW spinlocks on the device unless
this API is used to set aside specific spinlocks for use outside
of IPC.
Instance Config Parameters |
|
XDCscript usage |
meta-domain |
var params = new GateHWSpinlock.Params;
// Instance config-params object
params.resourceId = UInt 0;
// Logical resource id
params.sharedAddr = Ptr null;
// Physical address of the shared memory
config GateHWSpinlock.resourceId // instance |
|
Logical resource id
XDCscript usage |
meta-domain |
var params = new GateHWSpinlock.Params;
...
params.resourceId = UInt 0;
C SYNOPSIS
config GateHWSpinlock.sharedAddr // instance |
|
Physical address of the shared memory
XDCscript usage |
meta-domain |
var params = new GateHWSpinlock.Params;
...
params.sharedAddr = Ptr null;
DETAILS
This parameter is only used by GateMP delegates that use shared memory
C SYNOPSIS
Instance Creation |
|
XDCscript usage |
meta-domain |
var params =
new GateHWSpinlock.
Params;
// Allocate instance config-params
params.config = ...
// Assign individual configs
// Create an instance-object
ARGUMENTS
localGate
Gate to use for local protection.
params
per-instance config params, or NULL to select default values (target-domain only)
eb
active error-handling block, or NULL to select default policy (target-domain only)
DETAILS
A Non-NULL gate for local protection must be passed to the create
call. If no local protection is desired, a
xdc.runtime.GateNull handle must be passed in.