| module ti.sdo.ipc.SharedRegion |
 |
 |
Shared memory manager and address translator
This module has a common header that can be found in the
ti.ipc
package. Application code should include the common header file (not the
RTSC-generated one):
#include <ti/ipc/SharedRegion.h>
The RTSC module must be used in the application's RTSC configuration file
(.cfg) if runtime APIs will be used in the application:
SharedRegion = xdc.useModule('ti.sdo.ipc.SharedRegion');
Documentation for all runtime APIs, instance configuration parameters,
error codes macros and type definitions available to the application
integrator can be found in the
Doxygen documenation
for the IPC product. However, the documentation presented on this page
should be referred to for information specific to the RTSC module, such as
module configuration, Errors, and Asserts.
[
more ... ]
#include <ti/sdo/ipc/SharedRegion.h>
Functions common to all target modules |
|
|
Defines |
#define | |
#define | |
Typedefs |
typedef struct | |
typedef Bits32 | |
Constants |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
extern const SizeT | |
extern const UInt16 | |
extern const Bool | |
DETAILS
This module has a common header that can be found in the
ti.ipc
package. Application code should include the common header file (not the
RTSC-generated one):
#include <ti/ipc/SharedRegion.h>
The RTSC module must be used in the application's RTSC configuration file
(.cfg) if runtime APIs will be used in the application:
SharedRegion = xdc.useModule('ti.sdo.ipc.SharedRegion');
Documentation for all runtime APIs, instance configuration parameters,
error codes macros and type definitions available to the application
integrator can be found in the
Doxygen documenation
for the IPC product. However, the documentation presented on this page
should be referred to for information specific to the RTSC module, such as
module configuration, Errors, and Asserts.
The SharedRegion module is designed to be used in a multi-processor
environment in which memory regions are shared and accessed
across different processors. The module itself does not use any shared
memory, because all module state is stored locally. SharedRegion
APIs use the system gate for thread protection.
This module creates and stores a local shared memory region table. The
table contains the processor's view for every shared region in the system.
The table must not contain any overlapping regions. Each processor's
view of a particular shared memory region is determined by the region id.
In cases where a processor cannot access a certain shared memory region,
that shared memory region should be left invalid for that processor.
Note: The
numEntries must be the same on all processors.
Each shared region contains the following:
- base: The base address
- len: The length
- name: The name of the region
- isValid: Whether the region is valid
- ownerProcId: The id of the processor which owns the region
- cacheEnable: Whether the region is cacheable
- cacheLineSize: The cache line size
- createHeap: Whether a heap is created for the region.
A region is added statically using the
setEntryMeta API.
The length of a region must be the same across all processors.
The owner of the region can be specified. If specified, the owner
manages the shared region. It creates a HeapMemMP instance which spans
the full size of the region. The other processors open the same HeapMemMP
instance.
Note: Prior to calling Ipc_start(), If a SharedRegion's 'isValid'
is true and 'createHeap' is true then the owner of the SharedRegion
must be the same as the owner of SharedRegion 0.
An example of a SharedRegion configuration is as follows:
var SharedRegion = xdc.useModule('ti.sdo.ipc.SharedRegion');
SharedRegion.setEntryMeta(0,
{ base: 0x80000000,
len: 0x20000,
ownerProcId: 0,
isValid: true,
cacheLineSize: 64,
name: "DDR2",
});
The shared region table along with a shared region pointer (SRPtr)
is used to do address translation at runtime. The shared region
pointer is a 32-bit portable pointer composed of an id and offset.
The most significant bits of a SRPtr are used for the id.
The id corresponds to the index of the entry in the table.
The offset is the offset from the base of the shared memory region.
The number of entries in the table determines the number of bits to
use for the id. Increasing the number of entries increases the
range of ids but decreases the range of the offset.
Note: Region 0 must be visible by all processors. Region 0 is used for
synchonizing the processors, creating the default GateMP, and
creating Notify and MessageQ transport instances. The HeapMemMP
created in Region 0 is the length of the region minus memory
reserved for creating these internal instances.
Refer to the doxygen documentation for run-time API documenation.
| const SharedRegion_DEFAULTOWNERID |
 |
Specifies the default owner proc id
#define SharedRegion_DEFAULTOWNERID (UInt16)~0
| const SharedRegion_INVALIDREGIONID |
 |
Specifies the invalid id
#define SharedRegion_INVALIDREGIONID (UInt16)0xFFFF
| typedef SharedRegion_SRPtr |
 |
Definition of shared region pointer type
typedef Bits32 SharedRegion_SRPtr;
| struct SharedRegion_Entry |
 |
Structure for specifying a region
typedef struct SharedRegion_Entry {
Ptr base;
SizeT len;
UInt16 ownerProcId;
Bool isValid;
Bool cacheEnable;
SizeT cacheLineSize;
Bool createHeap;
String name;
} SharedRegion_Entry;
FIELDS
base
The base address.
len
The length.
ownerProcId
MultiProc id of processor that manages region.
isValid
Whether the region is valid or not.
cacheEnable
Whether the region is cacheable.
cacheLineSize
The cache line size for the region.
createHeap
Whether a heap is created for the region.
name
The name associated with the region.
DETAILS
Each region entry should not overlap with any other entry. The
length of a region should be the same across all processors.
During static configuration, the 'isValid' field can be set to 'false'
to signify a partially completed entry. This should only be done
if the base address of the entry is not known during static
configuration. The entry can be completed and the
'isValid' field can be set to true at runtime.
| config SharedRegion_A_addrOutOfRange // module-wide |
 |
Assert raised when an address is out of the range of the region id
extern const Assert_Id SharedRegion_A_addrOutOfRange;
| config SharedRegion_A_alreadyExists // module-wide |
 |
Assert raised when a valid table entry already exists
extern const Assert_Id SharedRegion_A_alreadyExists;
| config SharedRegion_A_cacheLineSizeIsZero // module-wide |
 |
Assert raised when cache enabled but cache line size = 0
extern const Assert_Id SharedRegion_A_cacheLineSizeIsZero;
| config SharedRegion_A_idTooLarge // module-wide |
 |
Assert raised when the id is larger than numEntries
extern const Assert_Id SharedRegion_A_idTooLarge;
| config SharedRegion_A_noHeap // module-wide |
 |
Assert raised when trying to use a heap for a region that has no heap
extern const Assert_Id SharedRegion_A_noHeap;
| config SharedRegion_A_overlap // module-wide |
 |
Assert raised when a new entry overlaps an existing one
extern const Assert_Id SharedRegion_A_overlap;
| config SharedRegion_A_region0Clear // module-wide |
 |
Assert raised when attempting to clear region 0
extern const Assert_Id SharedRegion_A_region0Clear;
| config SharedRegion_A_region0Invalid // module-wide |
 |
Assert raised when region zero is invalid
extern const Assert_Id SharedRegion_A_region0Invalid;
| config SharedRegion_A_regionInvalid // module-wide |
 |
Assert raised when region is invalid
extern const Assert_Id SharedRegion_A_regionInvalid;
| config SharedRegion_A_reserveTooMuch // module-wide |
 |
Assert raised when the trying to reserve too much memory
extern const Assert_Id SharedRegion_A_reserveTooMuch;
| config SharedRegion_cacheLineSize // module-wide |
 |
Worst-case cache line size
extern const SizeT SharedRegion_cacheLineSize;
DETAILS
This is the default system cache line size for all modules.
When a module puts structures in shared memory, this value is
used to make sure items are aligned on a cache line boundary.
If no cacheLineSize is specified for a region, it will use this
value.
| config SharedRegion_numEntries // module-wide |
 |
The number of shared region table entries
extern const UInt16 SharedRegion_numEntries;
DETAILS
This value is used for calculating the number of bits for the offset.
Note: This value must be the same across all processors in the system.
Increasing this parameter will increase the footprint and
the time for translating a pointer to a SRPtr.
| config SharedRegion_translate // module-wide |
 |
Determines whether address translation is required
extern const Bool SharedRegion_translate;
DETAILS
This configuration parameter should be set to 'false' if and only if all
shared memory regions have the same base address for all processors.
If 'false', it results in a fast
getPtr and
getSRPtr,
because a SRPtr is equivalent to a Ptr and no translation is done.
| Module-Wide Built-Ins |
 |
// Get this module's unique id
Bool SharedRegion_Module_startupDone();
// Test if this module has completed startup
// The heap from which this module allocates memory
Bool SharedRegion_Module_hasMask();
// Test whether this module has a diagnostics mask
Bits16 SharedRegion_Module_getMask();
// Returns the diagnostics mask for this module
Void SharedRegion_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
var SharedRegion = xdc.useModule('ti.sdo.ipc.SharedRegion');
module-wide constants & types
module-wide config parameters
msg: "A_addrOutOfRange: Address is out of region id's range"
};
msg: "A_alreadyExists: Trying to overwrite an existing valid entry"
};
msg: "A_cacheLineSizeIsZero: cache line size cannot be zero"
};
msg: "A_idTooLarge: id cannot be larger than numEntries"
};
msg: "A_noHeap: Region has no heap"
};
msg: "A_overlap: Shared region overlaps"
};
msg: "A_region0Clear: Region 0 cannot be cleared"
};
msg: "A_region0Invalid: Region zero is invalid"
};
msg: "A_regionInvalid: Region is invalid"
};
msg: "A_reserveTooMuch: Trying to reserve too much memory"
};
module-wide functions
| const SharedRegion.DEFAULTOWNERID |
 |
Specifies the default owner proc id
| XDCscript usage |
meta-domain |
const SharedRegion.DEFAULTOWNERID = ~0;
C SYNOPSIS
| const SharedRegion.INVALIDREGIONID |
 |
Specifies the invalid id
| XDCscript usage |
meta-domain |
const SharedRegion.INVALIDREGIONID = 0xFFFF;
C SYNOPSIS
| struct SharedRegion.Entry |
 |
Structure for specifying a region
| XDCscript usage |
meta-domain |
var obj = new SharedRegion.Entry;
obj.base = Ptr ...
obj.len = SizeT ...
obj.ownerProcId = UInt16 ...
obj.isValid = Bool ...
obj.cacheEnable = Bool ...
obj.cacheLineSize = SizeT ...
obj.createHeap = Bool ...
obj.name = String ...
FIELDS
base
The base address.
len
The length.
ownerProcId
MultiProc id of processor that manages region.
isValid
Whether the region is valid or not.
cacheEnable
Whether the region is cacheable.
cacheLineSize
The cache line size for the region.
createHeap
Whether a heap is created for the region.
name
The name associated with the region.
DETAILS
Each region entry should not overlap with any other entry. The
length of a region should be the same across all processors.
During static configuration, the 'isValid' field can be set to 'false'
to signify a partially completed entry. This should only be done
if the base address of the entry is not known during static
configuration. The entry can be completed and the
'isValid' field can be set to true at runtime.
C SYNOPSIS
| config SharedRegion.A_addrOutOfRange // module-wide |
 |
Assert raised when an address is out of the range of the region id
| XDCscript usage |
meta-domain |
msg: "A_addrOutOfRange: Address is out of region id's range"
};
C SYNOPSIS
| config SharedRegion.A_alreadyExists // module-wide |
 |
Assert raised when a valid table entry already exists
| XDCscript usage |
meta-domain |
msg: "A_alreadyExists: Trying to overwrite an existing valid entry"
};
C SYNOPSIS
| config SharedRegion.A_cacheLineSizeIsZero // module-wide |
 |
Assert raised when cache enabled but cache line size = 0
| XDCscript usage |
meta-domain |
msg: "A_cacheLineSizeIsZero: cache line size cannot be zero"
};
C SYNOPSIS
| config SharedRegion.A_idTooLarge // module-wide |
 |
Assert raised when the id is larger than numEntries
| XDCscript usage |
meta-domain |
msg: "A_idTooLarge: id cannot be larger than numEntries"
};
C SYNOPSIS
| config SharedRegion.A_noHeap // module-wide |
 |
Assert raised when trying to use a heap for a region that has no heap
| XDCscript usage |
meta-domain |
msg: "A_noHeap: Region has no heap"
};
C SYNOPSIS
| config SharedRegion.A_overlap // module-wide |
 |
Assert raised when a new entry overlaps an existing one
| XDCscript usage |
meta-domain |
msg: "A_overlap: Shared region overlaps"
};
C SYNOPSIS
| config SharedRegion.A_region0Clear // module-wide |
 |
Assert raised when attempting to clear region 0
| XDCscript usage |
meta-domain |
msg: "A_region0Clear: Region 0 cannot be cleared"
};
C SYNOPSIS
| config SharedRegion.A_region0Invalid // module-wide |
 |
Assert raised when region zero is invalid
| XDCscript usage |
meta-domain |
msg: "A_region0Invalid: Region zero is invalid"
};
C SYNOPSIS
| config SharedRegion.A_regionInvalid // module-wide |
 |
Assert raised when region is invalid
| XDCscript usage |
meta-domain |
msg: "A_regionInvalid: Region is invalid"
};
C SYNOPSIS
| config SharedRegion.A_reserveTooMuch // module-wide |
 |
Assert raised when the trying to reserve too much memory
| XDCscript usage |
meta-domain |
msg: "A_reserveTooMuch: Trying to reserve too much memory"
};
C SYNOPSIS
| config SharedRegion.cacheLineSize // module-wide |
 |
Worst-case cache line size
| XDCscript usage |
meta-domain |
SharedRegion.cacheLineSize = SizeT 128;
DETAILS
This is the default system cache line size for all modules.
When a module puts structures in shared memory, this value is
used to make sure items are aligned on a cache line boundary.
If no cacheLineSize is specified for a region, it will use this
value.
C SYNOPSIS
| config SharedRegion.numEntries // module-wide |
 |
The number of shared region table entries
| XDCscript usage |
meta-domain |
SharedRegion.numEntries = UInt16 4;
DETAILS
This value is used for calculating the number of bits for the offset.
Note: This value must be the same across all processors in the system.
Increasing this parameter will increase the footprint and
the time for translating a pointer to a SRPtr.
C SYNOPSIS
| config SharedRegion.translate // module-wide |
 |
Determines whether address translation is required
| XDCscript usage |
meta-domain |
SharedRegion.translate = Bool true;
DETAILS
This configuration parameter should be set to 'false' if and only if all
shared memory regions have the same base address for all processors.
If 'false', it results in a fast
getPtr and
getSRPtr,
because a SRPtr is equivalent to a Ptr and no translation is done.
C SYNOPSIS
| metaonly config SharedRegion.common$ // module-wide |
 |
Common module configuration parameters
| XDCscript usage |
meta-domain |
DETAILS
All modules have this configuration parameter. Its name
contains the '$' character to ensure it does not conflict with
configuration parameters declared by the module. This allows
new configuration parameters to be added in the future without
any chance of breaking existing modules.
| metaonly SharedRegion.getCacheLineSizeMeta() // module-wide |
 |
Meta version of Ipc_getCacheLineSize
| XDCscript usage |
meta-domain |
SharedRegion.getCacheLineSizeMeta(UInt16 id) returns SizeT
| metaonly SharedRegion.setEntryMeta() // module-wide |
 |
Sets the entry at the specified region id in the shared region table
| XDCscript usage |
meta-domain |
ARGUMENTS
id
Region id.
entry
Entry fields about the region.
DETAILS
The required parameters are base and len. All the other fields will
get their default if not specified.
generated on Sat, 11 Feb 2012 00:38:10 GMT