![]() |
![]() |
Structure defining parameters for the MessageQ module. More...
#include <MessageQ.h>
Data Fields | |
Void * | synchronizer |
Structure defining parameters for the MessageQ module.
Synchronizer instance used to signal IO completion
The synchronizer is used in the MessageQ_put and MessageQ_get calls. The synchronizer signal is called as part of the MessageQ_put call. The synchronizer waits in the MessageQ_get if there are no messages present.