HeapMemMP.h File Reference


Detailed Description

Multi-processor variable size buffer heap implementation.

============================================================================

HeapMemMP is a heap implementation that manages variable size buffers that can be used in a multiprocessor system with shared memory. HeapMemMP manages a single buffer in shared memory from which blocks of user- specified length are allocated and freed.

The HeapMemMP module uses a NameServer instance to store instance information when an instance is created. The name supplied must be unique for all HeapMemMP instances.

The HeapMemMP_create call initializes the shared memory as needed. Once an instance is created, an HeapMemMP_open can be performed. The open is used to gain access to the same HeapMemMP instance. Generally an instance is created on one processor and opened on the other processor(s).

The open returns a HeapMemMP instance handle like the create, however the open does not modify the shared memory.

Because HeapMemMP is a variable-size heap implementation, it is also used by the SharedRegion module to manage shared memory in each shared region. When any shared memory IPC instance is created in a particular shared region, the HeapMemMP that manages shared memory in the shared region allocates shared memory for the instance.

The HeapMemMP header should be included in an application as follows:

  #include <ti/ipc/HeapMemMP.h>
Version:
0.00.01

============================================================================

#include <ti/ipc/GateMP.h>
Include dependency graph for HeapMemMP.h:

Go to the source code of this file.

Data Structures

struct  HeapMemMP_Params
 Structure defining parameters for the HeapMemMP module. More...
struct  HeapMemMP_ExtendedStats
 Stats structure for the HeapMemMP_getExtendedStats API. More...

Defines

#define HeapMemMP_S_BUSY   2
 The resource is still in use.
#define HeapMemMP_S_ALREADYSETUP   1
 The module has been already setup.
#define HeapMemMP_S_SUCCESS   0
 Operation is successful.
#define HeapMemMP_E_FAIL   -1
 Generic failure.
#define HeapMemMP_E_INVALIDARG   -2
 Argument passed to function is invalid.
#define HeapMemMP_E_MEMORY   -3
 Operation resulted in memory failure.
#define HeapMemMP_E_ALREADYEXISTS   -4
 The specified entity already exists.
#define HeapMemMP_E_NOTFOUND   -5
 Unable to find the specified entity.
#define HeapMemMP_E_TIMEOUT   -6
 Operation timed out.
#define HeapMemMP_E_INVALIDSTATE   -7
 Module is not initialized.
#define HeapMemMP_E_OSFAILURE   -8
 A failure occurred in an OS-specific call.
#define HeapMemMP_E_RESOURCE   -9
 Specified resource is not available.
#define HeapMemMP_E_RESTART   -10
 Operation was interrupted. Please restart the operation.

Typedefs

typedef struct HeapMemMP_Object * HeapMemMP_Handle
 HeapMemMP_Handle type.

Functions

Int HeapMemMP_close (HeapMemMP_Handle *handlePtr)
 Close a HeapMemMP instance.
HeapMemMP_Handle HeapMemMP_create (const HeapMemMP_Params *params)
 Create a HeapMemMP instance.
Int HeapMemMP_delete (HeapMemMP_Handle *handlePtr)
 Delete a created HeapMemMP instance.
Int HeapMemMP_open (String name, HeapMemMP_Handle *handlePtr)
 Open a created HeapMemMP instance.
Void HeapMemMP_Params_init (HeapMemMP_Params *params)
 Initialize a HeapMemMP parameters struct.
Void * HeapMemMP_alloc (HeapMemMP_Handle handle, SizeT size, SizeT align)
 Allocate a block of memory of specified size and alignment.
Void HeapMemMP_free (HeapMemMP_Handle handle, Ptr block, SizeT size)
 Frees a block of memory.
Void HeapMemMP_getExtendedStats (HeapMemMP_Handle handle, HeapMemMP_ExtendedStats *stats)
 Get extended memory statistics.
Void HeapMemMP_getStats (HeapMemMP_Handle handle, Ptr stats)
 Get memory statistics.
Void HeapMemMP_restore (HeapMemMP_Handle handle)
 Restore an instance to it's original created state.

Define Documentation

#define HeapMemMP_S_BUSY   2

The resource is still in use.

#define HeapMemMP_S_ALREADYSETUP   1

The module has been already setup.

#define HeapMemMP_S_SUCCESS   0

Operation is successful.

#define HeapMemMP_E_FAIL   -1

Generic failure.

#define HeapMemMP_E_INVALIDARG   -2

Argument passed to function is invalid.

#define HeapMemMP_E_MEMORY   -3

Operation resulted in memory failure.

#define HeapMemMP_E_ALREADYEXISTS   -4

The specified entity already exists.

#define HeapMemMP_E_NOTFOUND   -5

Unable to find the specified entity.

#define HeapMemMP_E_TIMEOUT   -6

Operation timed out.

#define HeapMemMP_E_INVALIDSTATE   -7

Module is not initialized.

#define HeapMemMP_E_OSFAILURE   -8

A failure occurred in an OS-specific call.

#define HeapMemMP_E_RESOURCE   -9

Specified resource is not available.

#define HeapMemMP_E_RESTART   -10

Operation was interrupted. Please restart the operation.


Typedef Documentation

typedef struct HeapMemMP_Object* HeapMemMP_Handle

HeapMemMP_Handle type.


Function Documentation

Int HeapMemMP_close ( HeapMemMP_Handle handlePtr  ) 

Close a HeapMemMP instance.

Closing an instance will free local memory consumed by the opened instance. All opened instances should be closed before the instance is deleted.

Parameters:
[in,out] handlePtr Pointer to handle returned from HeapMemMP_open
HeapMemMP_Handle HeapMemMP_create ( const HeapMemMP_Params params  ) 

Create a HeapMemMP instance.

Parameters:
[in] params HeapMemMP parameters
Returns:
HeapMemMP Handle
Int HeapMemMP_delete ( HeapMemMP_Handle handlePtr  ) 

Delete a created HeapMemMP instance.

Parameters:
[in,out] handlePtr Pointer to handle to delete.
Int HeapMemMP_open ( String  name,
HeapMemMP_Handle handlePtr 
)

Open a created HeapMemMP instance.

Once an instance is created, an open can be performed. The open is used to gain access to the same HeapMemMP instance. Generally an instance is created on one processor and opened on the other processor.

The open returns a HeapMemMP instance handle like the create, however the open does not initialize the shared memory. The supplied name is used to identify the created instance.

Call HeapMemMP_close when the opened instance is not longer needed.

Parameters:
[in] name Name of created HeapMemMP instance
[out] handlePtr Pointer to HeapMemMP handle to be opened
Returns:
HeapMemMP status:
See also:
HeapMemMP_close
Void HeapMemMP_Params_init ( HeapMemMP_Params params  ) 

Initialize a HeapMemMP parameters struct.

Parameters:
[out] params Pointer to GateMP parameters
Void* HeapMemMP_alloc ( HeapMemMP_Handle  handle,
SizeT  size,
SizeT  align 
)

Allocate a block of memory of specified size and alignment.

The actual block returned may be larger than requested to satisfy alignment requirements.

HeapMemMP_alloc will lock the heap using the HeapMemMP gate while it traverses the list of free blocks to find a large enough block for the request.

Guidelines for using large heaps and multiple alloc() calls.

  • If possible, allocate larger blocks first. Previous allocations of small memory blocks can reduce the size of the blocks available for larger memory allocations.
  • Realize that alloc() can fail even if the heap contains a sufficient absolute amount of unalloccated space. This is because the largest free memory block may be smaller than total amount of unallocated memory.
Parameters:
[in] handle Handle to previously created/opened instance.
[in] size Size to be allocated (in MADUs)
[in] align Alignment for allocation (power of 2)
See also:
HeapMemMP_free
Void HeapMemMP_free ( HeapMemMP_Handle  handle,
Ptr  block,
SizeT  size 
)

Frees a block of memory.

free() places the memory block specified by addr and size back into the free pool of the heap specified. The newly freed block is combined with any adjacent free blocks. The space is then available for further allocation by alloc().

HeapMemMP_free will lock the heap using the HeapMemMP gate if one is specified or the system GateMP if not.

Parameters:
[in] handle Handle to previously created/opened instance.
[in] block Block of memory to be freed.
[in] size Size to be freed (in MADUs)
See also:
HeapMemMP_alloc
Void HeapMemMP_getExtendedStats ( HeapMemMP_Handle  handle,
HeapMemMP_ExtendedStats stats 
)

Get extended memory statistics.

This function retrieves extended statistics for a HeapMemMP instance. Refer to HeapMemMP_ExtendedStats for more information regarding what information is returned.

Parameters:
[in] handle Handle to previously created/opened instance.
[out] stats ExtendedStats structure
See also:
Void HeapMemMP_getStats ( HeapMemMP_Handle  handle,
Ptr  stats 
)

Get memory statistics.

Parameters:
[in] handle Handle to previously created/opened instance.
[out] stats Memory statistics structure
See also:
Void HeapMemMP_restore ( HeapMemMP_Handle  handle  ) 

Restore an instance to it's original created state.

This function restores an instance to its original created state. Any memory previously allocated from the heap is no longer valid after this API is called. This function does not check whether there is allocated memory or not.

Parameters:
[in] handle Handle to previously created/opened instance.

Copyright 2010, Texas Instruments Incorporated