![]() |
![]() |
Framework Components Application Programming Interface (API)
fc-u06
|
IRES_HDVICP_Obj extends the generic IRES_Obj structure that is returned back to the algorithm requesting the resource. More...
#include <ires_hdvicp.h>
Data Fields | |
IRES_Obj | ires |
Void * | info |
Int | id |
Void * | registerBaseAddress |
Void * | memoryBaseAddress |
unsigned int | pscRegisterSpace |
IRES_HDVICP_Obj extends the generic IRES_Obj structure that is returned back to the algorithm requesting the resource.
IRES_Obj IRES_HDVICP_Obj::ires |
Void* IRES_HDVICP_Obj::info |
RSVD for future use
Int IRES_HDVICP_Obj::id |
ID of the HDVICP being , granted, could be IRES_HDVICP_ID_0 or IRES_HDVICP_ID_1
Void* IRES_HDVICP_Obj::registerBaseAddress |
Base address of reg space
Void* IRES_HDVICP_Obj::memoryBaseAddress |
Mem address of mem space
unsigned int IRES_HDVICP_Obj::pscRegisterSpace |
Base address of the PSC and system module register space