const DMAN3.MAXGROUPS |
|
Maximum number of groups for sharing
TCCs and parameter RAM
XDCscript usage |
meta-domain |
const DMAN3.MAXGROUPS = 20;
config DMAN3.allowUnshared // module-wide |
|
Allow DMAN3-related resources to be granted to an algorithm, even
if there are not enough resources configured into the shared
groupId which the algorithm is a member of
XDCscript usage |
meta-domain |
DMAN3.allowUnshared = Bool true;
DETAILS
If this property is set to false, the DMAN3 library will fail
to grant DMA channels to an algorithm requesting more TCCs or
PaRams then the number configured for its scratch group.
If this property is true, and an algorithm requests more TCCs or
PaRams than the number configured for its scratch group, DMAN3 will
do either of the following:
- If no algorithm is currently instantiated for the given scratch
group, DMAN3 will bump up the number of TCCs and PaRams to the
maximum of the number configured and that requested by the
algorithm, for the scratch group. This will remain in effect
until all algorithms for that scratch group are deleted.
- If an algorithm has already been granted DMA channels for the
given scratch group (so the number of TCCs and PaRams for that
scratch group has already been determined by (1) above), and the
number of TCCs or PaRams for the scratch group is insufficient for
the algorithm currently requesting DMA channels, DMAN3 will
allocate new TCCs and PaRams if available. These new TCCs and
PaRams will not be shared by any other algorithm.
config DMAN3.cpu // module-wide |
|
Use the non-EDMA3, CPU version of DMAN3
XDCscript usage |
meta-domain |
config DMAN3.customDmaLib // module-wide |
|
Set this to TRUE if a custom library is being used to perform DMA
transfers. In this case, qdma channels will have to be partitioned
into scratch groups using the numQdmaGroup configuration
XDCscript usage |
meta-domain |
DMAN3.customDmaLib = Bool undefined;
config DMAN3.heapExternal // module-wide |
|
Heap ID for dyn allocation of private DMAN3 data structures
XDCscript usage |
meta-domain |
DMAN3.heapExternal = String null;
DETAILS
This parameter is unused when DMAN3 is used in a Linux environment.
This parameter is set to DMAN3_HEAP_EXTERNAL.
config DMAN3.heapInternal // module-wide |
|
Heap ID for dynamic allocation of DMAN3 objects
XDCscript usage |
meta-domain |
DMAN3.heapInternal = String null;
DETAILS
This must be allocated in L1D Internal RAM.
This parameter is unused when DMAN3 is used in a Linux environment.
This parameter is set to DMAN3_HEAP_INTERNAL.
config DMAN3.idma3Internal // module-wide |
|
Use the internal memory heap for dynamic allocation of IDMA3 objects
XDCscript usage |
meta-domain |
DMAN3.idma3Internal = Bool true;
DETAILS
A value of
false means that IDMA3 objects will be allocated
in the heap specified by
heapExternal. If the
value is
true, IDMA3 objects will be
allocated in the heap specified by
heapInternal.
config DMAN3.maxPaRamEntries // module-wide |
|
Total number of PARAM Table entries on the target hardware.
(eg, for IVA2, Davinci this is 128, for Himalaya, this is 256)
XDCscript usage |
meta-domain |
DMAN3.maxPaRamEntries = UInt 128;
DETAILS
This parameter is set to DMAN3_MAX_PARAM_ENTRIES.
config DMAN3.maxQdmaChannels // module-wide |
|
The total number of Physical QDMA channels available on the
target hardware (eg, 8 for DaVinci, 4 for IVA2)
XDCscript usage |
meta-domain |
DMAN3.maxQdmaChannels = UInt 8;
DETAILS
This parameter is set to DMAN3_MAX_QDMA_CHANNELS.
config DMAN3.maxTCs // module-wide |
|
Maximum number of transfer controllers on this SOC
XDCscript usage |
meta-domain |
config DMAN3.nullPaRamIndex // module-wide |
|
Index of PaRam to be reserved as a "null" PaRam. This index will be
used to set QCHMAP when the corresponding QDMA channel is not active.
The value of nullPaRamIndex should be outside of the range of
PaRam indices alloted to DMAN3, i.e., nullPaRamIndex should be less
than paRamBaseIndex, or greater than paRamBaseIndex + numPaRamEntries.
If PaRam registers are shared between two processors (eg, an Arm
and a DSP), make sure the nullPaRamIndex is not used by the other
processor
XDCscript usage |
meta-domain |
DMAN3.nullPaRamIndex = UInt 0;
DETAILS
This parameter is set to DMAN3_NULLPARAMINDEX.
config DMAN3.numPaRamEntries // module-wide |
|
Number of PARAM Table entries starting at DMAN3_PARAM_BASE_INDEX
assigned by configuration for exclusive DMAN3 allocation
XDCscript usage |
meta-domain |
DMAN3.numPaRamEntries = UInt 32;
DETAILS
This parameter is set to DMAN3_NUM_CONTIGUOUS_PARAM_ENTRIES.
config DMAN3.numPaRamGroup // module-wide |
|
Arrays containing the number of PaRam entries that will be assigned to
groups for sharing
XDCscript usage |
meta-domain |
0,
0,
0,
0,
0,
0,
0,
0,
0,
0,
0,
0,
0,
0,
0,
0,
0,
0,
0,
0
];
DETAILS
Channels created with a given group ID will use TCCs and PaRams
allocated for that group ID, and may share them with other channels
created with the same group ID.
This parameter is set to DMAN3_NUMPARAM_GROUP.
config DMAN3.numQdmaChannels // module-wide |
|
The number of Physical QDMA channels that are assigned to
DMAN3 via configuration. These channels will be granted either
as scratch or persistently as part of IDMA3 handles
XDCscript usage |
meta-domain |
DMAN3.numQdmaChannels = UInt 4;
DETAILS
This parameter is set to DMAN3_NUM_QDMA_CHANNELS.
config DMAN3.numQdmaGroup // module-wide |
|
Arrays containing the number of Qdma channels that will be assigned to
groups for sharing
XDCscript usage |
meta-domain |
DETAILS
This configuration is required ONLY if the application uses atleast one
custom (non-ACPY3) DMA library that will request QDMA channels from
DMAN3. In this case, the configuration param "customDmaLib" should be
set to true.
Channels created with a given group ID will use TCCs and PaRams
allocated for that grup ID, and may share them with other channels
created with the same group ID. Qdma channels may be shared across
algorithms and scratch groups if all algorithms use the same ACPY3
library. But if even one algorithm uses a custom DMA library, Qdma
channels should be distribued among scratch groups like other EDMA3
resources.
config DMAN3.numTccGroup // module-wide |
|
Arrays containing the number of TCC that will be assigned to groups for
sharing
XDCscript usage |
meta-domain |
0,
0,
0,
0,
0,
0,
0,
0,
0,
0,
0,
0,
0,
0,
0,
0,
0,
0,
0,
0
];
DETAILS
Channels created with a given group ID will use TCCs and PaRams
allocated for that group ID, and may share them with other channels
created with the same group ID.
This parameter is set to DMAN3_NUMTCC_GROUP.
config DMAN3.paRamBaseIndex // module-wide |
|
(0 > value > 255) represents the first PARAM TABLE ENTRY NUMBER
that is assigned by configuration for exclusive DMAN3 allocation
XDCscript usage |
meta-domain |
DMAN3.paRamBaseIndex = UInt 96;
DETAILS
Typically, addresses (PaRam sets) between 0 and 63 are reserved for use
by drivers that need EDMA/chaining capabilities.
Additionally, on some multi-core devices (e.g. DM644x), PaRams are
shared between the different cores (e.g. ARM and C64+). In these
cases, an executable will be configured for each core, and each
executable should configure only the DMAN3 resources which will be used
on that core. E.g., on DM644x, the C64+ executable should
be configured to avoid using what the ARM uses. Note that on
OMAP2430, the ARM doesn't have access to EDMA so all PaRam sets
are available for the C64+ device.
This parameter is set to DMAN3_PARAM_BASE_INDEX.
config DMAN3.qdmaChannels // module-wide |
|
Array containing list of physical QDMA channels assigned to DMAN3
XDCscript usage |
meta-domain |
DMAN3.qdmaChannels = UInt[] [
0,
1,
2,
3
];
DETAILS
This array is of size
DMAN3_NUM_QDMA_CHANNELS
(configured by
numQdmaChannels).
This parameter is set to DMAN3_QDMA_CHANNELS[].
SEE
config DMAN3.qdmaPaRamBase // module-wide |
|
Physical base address of the PARAM0 in the EDMA3/QDMA
hardware whose resources are being managed by DMAN3
XDCscript usage |
meta-domain |
DMAN3.qdmaPaRamBase = Ptr 0x01C04000;
DETAILS
This parameter is set to DMAN3_QDMA_PARAM_BASE.
config DMAN3.qdmaQueueMap // module-wide |
|
Array contaning the mapping from QDMA Channels to Event Queues
XDCscript usage |
meta-domain |
DMAN3.qdmaQueueMap = UInt[] [
1,
1,
1,
1,
1,
1,
1,
1
];
DETAILS
Indicates mapping of all "qdmaChannels" defined above to
particular Event Queue. For example, channelQueueMap[0]
specifies queue number for qdmaChannel[0], etc.
Defaults map all qdmaChannels to Queue# 1
config DMAN3.queuePri // module-wide |
|
Array contaning priorities of the event queues
XDCscript usage |
meta-domain |
DMAN3.queuePri = UInt[] [
3,
7,
0,
0,
0,
0,
0,
0
];
DETAILS
Indicates the priority accorded to each physical event queue.
config DMAN3.queueTCMap // module-wide |
|
Array contaning the mapping from Event Queues to Transfer Controllers
XDCscript usage |
meta-domain |
DMAN3.queueTCMap = UInt[] [
0,
1,
2,
3,
4,
5,
6,
7
];
DETAILS
Indicates mapping of individual hardware Event Queues to the Transfer
Controllers.
config DMAN3.scratchAllocFxn // module-wide |
|
Function for allocating IDMA3 channel object's "env" in scratch
memory
XDCscript usage |
meta-domain |
DMAN3.scratchAllocFxn = String null;
config DMAN3.scratchFreeFxn // module-wide |
|
Function for freeing IDMA3 channel object's "env" that was allocated
in scratch memory
XDCscript usage |
meta-domain |
DMAN3.scratchFreeFxn = String null;
config DMAN3.tccAllocationMaskH // module-wide |
|
32-bit bitmask representing configuration provided list of TCCs
for exclusive DMAN3 allocation
XDCscript usage |
meta-domain |
DMAN3.tccAllocationMaskH = UInt 0xffffffff;
DETAILS
For example, for TCC's in the range 0-31 the Low Mask
(tccAllocationMaskL) is configured so that a '1' in bit position 'i'
indicates the TCC 'i' is assigned to DMAN3.
This parameter is set to DMAN3_TCC_FREEMASK_H.
config DMAN3.tccAllocationMaskL // module-wide |
|
32-bit bitmask representing configuration provided list of TCCs
for exclusive DMAN3 allocation
XDCscript usage |
meta-domain |
DMAN3.tccAllocationMaskL = UInt 0x00000000;
DETAILS
For example, for TCC's in the range 0-31 the Low Mask
(tccAllocationMaskL) is configured so that a '1' in bit position 'i'
indicates the TCC 'i' is assigned to DMAN3.
This parameter is set to DMAN3_TCC_FREEMASK_L.
config DMAN3.useExternalRM // module-wide |
|
Boolean flag indicating if the EDMA3 Low Level
Resource Manager should be used to manage EDMA3
resources. If this flag is set to true, the SOC
specific settings are not required to be set in
this module. The ti.sdo.fc.edma3.Settings module
should be set up correctly
XDCscript usage |
meta-domain |
DMAN3.useExternalRM = Bool false;