metaonly module ti.sdo.fc.acpy3.ACPY3 |
EDMA3 "Algorithm Copy" library
usage | meta-domain | sourced in ti/sdo/fc/acpy3/ACPY3.xdc |
config ACPY3.cpu // module-wide |
Builds a non-EDMA, CPU only version of the library
usage | meta-domain |
config ACPY3.edma3BaseAddress // module-wide |
EDMA3 Base Address for the device Not required to be set if this library is used alongwith DMAN3
usage | meta-domain |
config ACPY3.enableLog // module-wide |
usage | meta-domain |
config ACPY3.nullPaRam // module-wide |
Index of the paRam to be used as Null paRam Not required to be set if this library is used alongwith DMAN3
usage | meta-domain |
config ACPY3.paRamBaseAddress // module-wide |
PaRam Base Address for the device Not required to be set if this library is used alongwith DMAN3 or for built for TI targets
usage | meta-domain |