![]() |
![]() |
IRES_VICP2_Obj extends the generic IRES_Obj structure that is returned back to the algorithm requesting the resource. More...
#include <ires_vicp2.h>
Data Fields | |
IRES_Obj | ires |
short | assignedIMX0 |
short | assignedIMX1 |
short | assignedMJCP |
short | assignedNSF |
unsigned int | assignedIMCOPBuffers [16] |
short | numMemBufs |
unsigned int | assignedMemAddrs [16] |
unsigned int | assignedMemSizes [16] |
unsigned int | configBaseAddress |
unsigned int | dmaViewConfigBaseAddr |
unsigned int | pscRegisterSpace |
IRES_VICP2_Obj extends the generic IRES_Obj structure that is returned back to the algorithm requesting the resource.
Value of 1 to indicate resource was granted, 0 otherwise
unsigned int IRES_VICP2_Obj::assignedIMCOPBuffers[16] |
Addresses of Named buffers granted, index array with IMCOP_BUFFER_<>
Number of individual memory buffers assigned
unsigned int IRES_VICP2_Obj::assignedMemAddrs[16] |
Addresses of buffers assigned, only the first numBufs will hold valid addresses
unsigned int IRES_VICP2_Obj::assignedMemSizes[16] |
unsigned int IRES_VICP2_Obj::configBaseAddress |
Base address of config space
unsigned int IRES_VICP2_Obj::dmaViewConfigBaseAddr |
Base address of DMA view of VICP buffers
unsigned int IRES_VICP2_Obj::pscRegisterSpace |
Base address of the PSC and system module register space