![]() |
![]() |
Functions | |
Int | DMAN3_grantDmaChannels (Int groupId, IALG_Handle algHandle[], IDMA3_Fxns *dmaFxns[], Int numAlgs) |
Add one or several algorithms to the DMA Manager. The DMA Manager will grant DMA resources to the algorithms as a result. This function is called when initializing XDAIS algorithm instances. | |
Void | DMAN3_exit (Void) |
Finalization method of the DMAN module. | |
Int | DMAN3_createChannels (Int groupId, IDMA3_ChannelRec dmaTab[], Int numChans) |
Allocate and initialize memory for one or several channel handles. | |
Void | DMAN3_init (Void) |
Initialization method of the DMAN3 module. DMAN3_init() uses externally configured and provided DMAN3_PARAMS to initialize DMAN3 resources (QDMA channel map, memory heap...) | |
Int | DMAN3_releaseDmaChannels (IALG_Handle algHandle[], IDMA3_Fxns *dmaFxns[], Int numAlgs) |
Remove logical channel resources from one or several algorithm instances. | |
Int | DMAN3_freeChannels (IDMA3_Handle channelTab[], Int numChans) |
Free memory for array of channel handles. | |
Defines | |
#define | DMAN3_MODNAME "ti.sdo.fc.dman3" |
Name to pass to Diags_setMask() to enable logging for DMAN3 functions. For example, Diags_setMask(DMAN3_MODNAME"+EX1234567"); turns on all Log statements in this module. Diags_setMask() must be called after initialization to take effect. | |
#define | DMAN3_GTNAME "ti.sdo.fc.dman3" |
#define | DMAN3_MAXGROUPS 20 |
Data Structures | |
struct | DMAN3_Params |
The module configuration structure for DMAN3 implementation. It is set at design time by the system integrator to ensure optimal sharing of DMA resources for the execution environment. More... | |
Typedefs | |
typedef Bool(* | DMAN3_ScratchAllocFxn )(IALG_Handle alg, Int mutexId, IALG_MemRec *memTab, Int numRecs) |
Function prototype for allocating IDMA3 Object's env from shared scratch memory. Algorithms might specify a particular IDMA3 protocol that provides custom DMA services. This protocol might require extra memory for the IDMA3 object's environment. DMAN3_ScratchAllocFxn might be used to allocate this memory. If this is NULL, then the env will be allocated from persistent memory. | |
typedef Void(* | DMAN3_ScratchFreeFxn )(Int mutexId, Void *addr, Uns size) |
Function prototype for freeing IDMA3 Object's env from shared scratch memory. If this is NULL then env will be freed from persistent memory. | |
typedef struct DMAN3_Params | DMAN3_Params |
The module configuration structure for DMAN3 implementation. It is set at design time by the system integrator to ensure optimal sharing of DMA resources for the execution environment. | |
Variables | |
DMAN3_Params | DMAN3_PARAMS |
Default module configuration structure (defined in dman3.c). | |
Uns | ti_sdo_fc_dman3_DMAN3_numQdmaGroup [20+1] |
Array containing the number of Qdma channels that will be assigned to the algorithm groups for sharing. | |
Bool | ti_sdo_fc_dman3_DMAN3_useCustomDma |
Flag indicating if custom DMA library is being used. | |
Defines: DMAN3 Status Codes | |
#define | DMAN3_SOK 0 |
#define | DMAN3_EOUTOFMEMORY -1 |
#define | DMAN3_EFAIL -2 |
#define | DMAN3_EFREE -3 |
#define | DMAN3_EOUTOFTCCS -4 |
#define | DMAN3_EOUTOFPARAMS -5 |
#define | DMAN3_ETCCCONFIG -6 |
#define | DMAN3_EPARAMCONFIG -7 |
DMAN3 is an application interface to the 3rd generation DMA Manager. It provides routines for granting and reclaiming DMA resources used by algorithms or other non-algorithm users. This module is used by frameworks or applications which have XDAIS algorithms that implement the IDMA3 interface.
Int DMAN3_grantDmaChannels | ( | Int | groupId, |
IALG_Handle | algHandle[], | ||
IDMA3_Fxns * | dmaFxns[], | ||
Int | numAlgs | ||
) |
Add one or several algorithms to the DMA Manager. The DMA Manager will grant DMA resources to the algorithms as a result. This function is called when initializing XDAIS algorithm instances.
[in] | groupId | Group number for sharing TCCs and PaRAMs. Channels created with the same group number in a previous or subsequent call to this function will share the same TCCs and PaRam, as the channels created in this call, so they must be used simultaneously. The channels created in this function call, will not share TCCs and PaRam with eachother, even though they use the same group Id. When granting DMA resources for several algorithms (i.e. when numAlgs is greater than 1) these algorithms do not share TCCs and PaRAMs. If two algorithms can share TCCs and PaRAMs, two calls to DMAN3_grantDmaChannels() are needed. |
[in] | algHandle[] | Array of algorithm handles. |
[in] | dmaFxns[] | Array of IDMA3 Interfaces associated with each algorithm handle. |
[in] | numAlgs | Number of algorithms in algHandle array. |
DMAN3_SOK | Success. |
DMAN3_EOUTOFMEMORY | Failed to allocate logical handle. |
DMAN3_EFAIL | Failed to initialize handle or dmaFxns dmaInit() failed. |
DMAN3_EOUTOFTCCS | Not enough TCCs available for channels. |
DMAN3_EOUTOFPARAMS | Not enough PaRams available for channels. |
IALG_Handle->fxns->implementationId == IDMA3_Fxns->implementationId
Void DMAN3_exit | ( | Void | ) |
Finalization method of the DMAN module.
Int DMAN3_createChannels | ( | Int | groupId, |
IDMA3_ChannelRec | dmaTab[], | ||
Int | numChans | ||
) |
Allocate and initialize memory for one or several channel handles.
[in] | groupId | Group number for sharing TCCs and PaRAMs. Channels created with the same group number in a previous or subsequent call to this function will share the same TCCs and PaRam, as the channels created in this call, so they must be used simultaneously. The channels created in this function call, will not share TCCs and PaRam with eachother, even though they use the same group Id. If two channels can share TCCs and PaRAMS then two calls to DMAN3_createChannels() are needed. |
[in] | dmaTab | Array of IDMA3 channel resource descriptors containing the parameters of the requested channels. |
[in] | numChans | Number of entries in dmaTab (ie, number of channels to create). |
[out] | dmaTab | On success assign valid and initialized IDMA3 logical DMA handle and environment (env, envSize) fields. |
DMAN3_SOK | Success. |
DMAN3_EOUTOFMEMORY | Failed to allocate logical handle. |
DMAN3_EFAIL | Failed to initialize handle or dmaFxns dmaInit() failed. |
DMAN3_EOUTOFTCCS | Not enough TCCs available for channels. |
DMAN3_EOUTOFPARAMS | Not enough PaRams available for channels. |
Void DMAN3_init | ( | Void | ) |
Initialization method of the DMAN3 module. DMAN3_init() uses externally configured and provided DMAN3_PARAMS to initialize DMAN3 resources (QDMA channel map, memory heap...)
Int DMAN3_releaseDmaChannels | ( | IALG_Handle | algHandle[], |
IDMA3_Fxns * | dmaFxns[], | ||
Int | numAlgs | ||
) |
Remove logical channel resources from one or several algorithm instances.
[in] | algHandle[] | Array of algorithm handles. |
[in] | dmaFxns[] | Array of IDMA3 Interfaces associated with the algorithm handles. |
[in] | numAlgs | Number of algorithm handles in algHandle[]. |
IALG_Handle->fxns->implementationId == IDMA2_Fxns->implementationId
Int DMAN3_freeChannels | ( | IDMA3_Handle | channelTab[], |
Int | numChans | ||
) |
Free memory for array of channel handles.
[in] | channelTab | Array of IDMA3 handles representing logical dma channel state. |
[in] | numChans | Number of entries in channelTab (ie, number of channels to free). |
DMAN3_SOK | Success. |
numChans
>= 0. #define DMAN3_MODNAME "ti.sdo.fc.dman3" |
Name to pass to Diags_setMask() to enable logging for DMAN3 functions. For example, Diags_setMask(DMAN3_MODNAME"+EX1234567"); turns on all Log statements in this module. Diags_setMask() must be called after initialization to take effect.
#define DMAN3_GTNAME "ti.sdo.fc.dman3" |
Name to identify the GT module
#define DMAN3_MAXGROUPS 20 |
Maximum number of groups for sharing TCCs and parameter RAM.
#define DMAN3_SOK 0 |
DMAN3 Status Code: Successful.
#define DMAN3_EOUTOFMEMORY -1 |
DMAN3 Status Code: Failed to allocate memory for the handle.
#define DMAN3_EFAIL -2 |
DMAN3 Status Code: Unspecified error.
#define DMAN3_EFREE -3 |
DMAN3 Status Code: Failed to free memory.
#define DMAN3_EOUTOFTCCS -4 |
DMAN3 Status Code: Insufficient number of TCCs available to create channels.
#define DMAN3_EOUTOFPARAMS -5 |
DMAN3 Status Code: Insufficient number of PaRams available to create channels.
#define DMAN3_ETCCCONFIG -6 |
DMAN3 Status Code: The number of TCCs configured for the scratchId is not enough to create the channels. This error can only be returned if allowUnshared
is set to FALSE.
#define DMAN3_EPARAMCONFIG -7 |
DMAN3 Status Code: The number of PaRams configured for the scratchId is not enough to create the channels. This error can only be returned if allowUnshared
is set to FALSE.
typedef Bool(* DMAN3_ScratchAllocFxn)(IALG_Handle alg, Int mutexId, IALG_MemRec *memTab, Int numRecs) |
Function prototype for allocating IDMA3 Object's env from shared scratch memory. Algorithms might specify a particular IDMA3 protocol that provides custom DMA services. This protocol might require extra memory for the IDMA3 object's environment. DMAN3_ScratchAllocFxn might be used to allocate this memory. If this is NULL, then the env will be allocated from persistent memory.
typedef Void(* DMAN3_ScratchFreeFxn)(Int mutexId, Void *addr, Uns size) |
Function prototype for freeing IDMA3 Object's env from shared scratch memory. If this is NULL then env will be freed from persistent memory.
typedef struct DMAN3_Params DMAN3_Params |
The module configuration structure for DMAN3 implementation. It is set at design time by the system integrator to ensure optimal sharing of DMA resources for the execution environment.
Default module configuration structure (defined in dman3.c).
Uns ti_sdo_fc_dman3_DMAN3_numQdmaGroup[20+1] |
Array containing the number of Qdma channels that will be assigned to the algorithm groups for sharing.
Flag indicating if custom DMA library is being used.