![]() |
![]() |
Functions | |
void | SCPY_init () |
SCPY initialization API. | |
void | SCPY_exit () |
SCPY finalization API. | |
void | SCPY_configure (IRES_SDMA_Handle logicalChannel, SCPY_Params *params) |
Configures transfer on a particular logical handle. | |
void | SCPY_start (IRES_SDMA_Handle logicalChannel) |
Starts a transfer previously configured on a channel. | |
void | SCPY_wait (IRES_SDMA_Handle logicalChannel) |
Wait for the transfer to complete. | |
Bool | SCPY_complete (IRES_SDMA_Handle logicalChannel) |
Returns status of transfer on the logical channel. | |
Defines | |
#define | OMAP_DMA_DATA_TYPE_S8 0x00 |
#define | OMAP_DMA_DATA_TYPE_S16 0x01 |
#define | OMAP_DMA_DATA_TYPE_S32 0x02 |
#define | OMAP_DMA_PORT_EMIFF 0x00 |
#define | OMAP_DMA_AMODE_POST_CONST 0x00 |
#define | OMAP_DMA_AMODE_POST_INC 0x01 |
#define | OMAP_DMA_AMODE_POST_SINGLE_INDEX 0x02 |
#define | OMAP_DMA_AMODE_POST_DOUBLE_INDEX 0x03 |
#define | OMAP_DMA_SYNC_MODE_ELEMENT 0x00 |
To identify mode of sychronization of transfer. | |
#define | OMAP_DMA_SYNC_MODE_FRAME 0x01 |
#define | OMAP_DMA_SYNC_MODE_BLOCK 0x02 |
#define | OMAP_DMA_SYNC_TYPE_DEST 0x00 |
#define | OMAP_DMA_SYNC_TYPE_SRC 0x01 |
Data Structures | |
struct | SCPY_AddrParams |
Parameters of Address (source or destination) of transfer. More... | |
struct | SCPY_TransferParams |
Details of Transfer. More... | |
struct | SCPY_Params |
Typedefs | |
typedef struct SCPY_AddrParams | SCPY_AddrParams |
Parameters of Address (source or destination) of transfer. | |
typedef struct SCPY_TransferParams | SCPY_TransferParams |
Details of Transfer. | |
typedef struct SCPY_Params | SCPY_Params |
The SCPY module provides a list of SDMA operations an algorithm can perform on logical SDMA channels it acquires through the IRES_SDMA protocol. Examples of SCPY operations include channel configuration, SDMA transfer scheduling, and SDMA transfer synchronization.
void SCPY_init | ( | ) |
SCPY initialization API.
void SCPY_exit | ( | ) |
SCPY finalization API.
void SCPY_configure | ( | IRES_SDMA_Handle | logicalChannel, |
SCPY_Params * | params | ||
) |
Configures transfer on a particular logical handle.
[in] | logicalChannel | Handle to the logical channel on which transfer will be configured |
[in] | params | Params to describe the transfer, src/dst addresses, sychronization mode, transfer dimensions etc. |
void SCPY_start | ( | IRES_SDMA_Handle | logicalChannel ) |
Starts a transfer previously configured on a channel.
[in] | logicalChannel | Previously configured logical channel on which to start the transfer. |
void SCPY_wait | ( | IRES_SDMA_Handle | logicalChannel ) |
Wait for the transfer to complete.
[in] | logicalChannel | Logical channel on which transfer is ongoing. |
Bool SCPY_complete | ( | IRES_SDMA_Handle | logicalChannel ) |
Returns status of transfer on the logical channel.
[in] | logicalChannel | Logical channel on which transfer is ongoing. |
TRUE | Transfer completed |
FALSE | Transfer in progress |
#define OMAP_DMA_DATA_TYPE_S8 0x00 |
#define OMAP_DMA_DATA_TYPE_S16 0x01 |
#define OMAP_DMA_DATA_TYPE_S32 0x02 |
#define OMAP_DMA_PORT_EMIFF 0x00 |
#define OMAP_DMA_AMODE_POST_CONST 0x00 |
#define OMAP_DMA_AMODE_POST_INC 0x01 |
#define OMAP_DMA_AMODE_POST_SINGLE_INDEX 0x02 |
#define OMAP_DMA_AMODE_POST_DOUBLE_INDEX 0x03 |
#define OMAP_DMA_SYNC_MODE_ELEMENT 0x00 |
To identify mode of sychronization of transfer.
#define OMAP_DMA_SYNC_MODE_FRAME 0x01 |
#define OMAP_DMA_SYNC_MODE_BLOCK 0x02 |
#define OMAP_DMA_SYNC_TYPE_DEST 0x00 |
#define OMAP_DMA_SYNC_TYPE_SRC 0x01 |
typedef struct SCPY_AddrParams SCPY_AddrParams |
Parameters of Address (source or destination) of transfer.
typedef struct SCPY_TransferParams SCPY_TransferParams |
Details of Transfer.
typedef struct SCPY_Params SCPY_Params |