![]() |
![]() |
Opaque client structure large enough to hold an instance object. More...
#include <RcmServer.h>
Data Fields | |
GateThread_Struct | _f1 |
Ptr | _f2 |
Ptr | _f3 |
Ptr | _f4 |
struct { | |
Int _f1 | |
Ptr _f2 | |
} | _f5 |
Ptr | _f6 [9] |
UInt16 | _f7 |
UInt16 | _f8 |
Bool | _f9 |
Int | _f10 |
Ptr | _f11 [4] |
Ptr | _f12 |
Opaque client structure large enough to hold an instance object.
Use this structure to define an embedded RcmServer object.
GateThread_Struct RcmServer_Struct::_f1 |
struct { ... } RcmServer_Struct::_f5 |
Ptr RcmServer_Struct::_f6[9] |
UInt16 RcmServer_Struct::_f7 |
UInt16 RcmServer_Struct::_f8 |
Ptr RcmServer_Struct::_f11[4] |