![]() |
![]() |
The module configuration structure for HDINTC implementation. More...
#include <hdintc.h>
Data Fields | |
int | interruptVectorId_0 |
Interrupt Vector 0. | |
int | interruptVectorId_1 |
Interrupt Vector 1. | |
int | hdvicpInterruptEventNo_0 |
Interrupt Event 0. | |
int | hdvicpInterruptEventNo_1 |
Interrupt Event 1. | |
int | biosInterruptVectorId_0 |
int | biosInterruptVectorId_1 |
int | biosInterruptEventNo_0 |
int | biosInterruptEventNo_1 |
The module configuration structure for HDINTC implementation.
Interrupt Vector 0.
Interrupt Vector 1.
Interrupt Event 0.
Interrupt Event 1.
======== biosInterruptVectorId_0 ======== Map this to an unused interrupt vector ID This vector Id is going to be used to set up a BIOS ISR
======== biosInterruptVectorId_1 ======== Map this to an unused interrupt vector ID This vector Id is going to be used to set up a BIOS ISR
======== biosInterruptEventNo_0 ======== This must correspond to an unused event on this device. This is a dummy event that will be mapped to the biosInterruptVectorId_0 above. This interrupt will be software triggered (by writing to the ISR). It won't be triggered by an actual event.
======== biosInterruptEventNo_1 ======== This must correspond to an unused event on this device. This is a dummy event that will be mapped to the biosInterruptVectorId_1 above. This interrupt will be software triggered (by writing to the ISR). It won't be triggered by an actual event.