IRES_TILEDMEMORY_Obj extends the generic IRES_Obj structure that is returned back to the algorithm requesting the resource. More...
#include <ires_tiledmemory.h>
Data Fields | |
IRES_Obj | ires |
XDAS_Void * | info |
XDAS_Void * | memoryBaseAddress |
XDAS_UInt32 | isTiledMemory |
XDAS_UInt32 | accessUnit |
XDAS_Void * | tilerBaseAddress |
XDAS_Void * | systemSpaceBaseAddress |
IRES_TILEDMEMORY_Obj extends the generic IRES_Obj structure that is returned back to the algorithm requesting the resource.
RSVD for future use
Process-specific virtual base address of Tiler memory allocated.
Boolean value that identifies if returned memory is of type TILED memory or not.
Valid values for this field are XDAS_TRUE and XDAS_FALSE.
If XDAS_TRUE, accessUnit will describe the kind of TILED memory allocated.
Describes the kind of memory actually allocated in the TILER space of type,
Base address of TILER on SOC
Tiler space base address of memory allocated