Static Resource Properties. More...
#include <ires_edma3Chan.h>
Data Fields | |
unsigned int | numDmaChannels |
unsigned int | numQdmaChannels |
unsigned int | numTccs |
unsigned int | numPaRAMSets |
unsigned int | numEvtQueue |
unsigned int | numTcs |
unsigned int | numRegions |
unsigned short | dmaChPaRAMMapExists |
Channel mapping existence. | |
unsigned short | memProtectionExists |
IRES_EDMA3CHAN_EDMA3RegisterLayer * | globalRegs |
Static Resource Properties.
unsigned int IRES_EDMA3CHAN_Properties::numDmaChannels |
Total number of DMA Channel supported by the EDMA3
unsigned int IRES_EDMA3CHAN_Properties::numQdmaChannels |
Total number of QDMA Channels supported by the EDMA3 Controller.
unsigned int IRES_EDMA3CHAN_Properties::numTccs |
Total number of Tccs supported by the EDMA3.
unsigned int IRES_EDMA3CHAN_Properties::numPaRAMSets |
Total number of PaRAM Sets supported by the EDMA3.
unsigned int IRES_EDMA3CHAN_Properties::numEvtQueue |
Total number of Event Queues in the EDMA3.
unsigned int IRES_EDMA3CHAN_Properties::numTcs |
Total number of Transfer Controllers (TCs) in the EDMA3 Controller.
unsigned int IRES_EDMA3CHAN_Properties::numRegions |
Number of Regions on the EDMA3 controller.
unsigned short IRES_EDMA3CHAN_Properties::dmaChPaRAMMapExists |
Channel mapping existence.
A value of 0 (No channel mapping) implies that there is fixed association for a channel number to a parameter entry number or, in other words, PaRAM entry n corresponds to channel n.
unsigned short IRES_EDMA3CHAN_Properties::memProtectionExists |
Existence of memory protection feature.
Pointer to Global Register region of CC Registers.