Instance create parameters. More...
#include <RcmClient.h>
Data Fields | |
UInt16 | heapId |
The heapId used by this instance for allocating messages. | |
Bool | callbackNotification |
Asynchronous callback notification support. |
Instance create parameters.
UInt16 RcmClient_Params::heapId |
The heapId used by this instance for allocating messages.
If sending messages to a remote server, the specified heap must be compatible with the transport used for delivering messages to the remote processor.
Asynchronous callback notification support.
When remote functions submitted with RcmClient_execAsync() complete, the given callback function is invoked. The callback function executes in the context of this RcmClient instance's callback server thread.
This config param must be set to true when using RcmClient_execAsync() to execute remote functions.
When set to false, the callback server thread is not created.