IRES generic Resource Manager RMAN Definitions - Generic Resource Manager that manages resource allocation for algorithms that implement the IRES interface.
Data Structures |
struct | RMAN_Params |
| The module configuration structure for RMAN. It is set at design time by the system integrator to register the specific Resource Managers(IRESMAN implementations). More...
|
struct | RMAN_YieldArgs |
| Yield Arguments passed to the algorithm if RMAN's useDSKT2 flag is set. These arguments are used by the yield function set/get context and release/acquire locks for a particular scratch group. More...
|
Defines |
#define | ti_sdo_fc_ires_NOPROTOCOLREV |
#define | RMAN_GTNAME "ti.sdo.fc.rman" |
| Name used to identify the GT module.
|
#define | RMAN_PROTOCOLNAMESIZE 200 |
| Size of the Protocol Name in the Resource Registry Table.
|
Typedefs |
typedef struct Sem_Obj * | RMAN_SemHandle |
| Declare abstract handle for Semaphore object.
|
Functions |
IRES_Status | RMAN_init (Void) |
| Initialize the RMAN object with static information from the headers/configuration etc. This function has to return successfully before the other APIs are called.
|
IRES_Status | RMAN_exit (Void) |
| Delete the generic IRES RMAN and release memory back.
|
IRES_Status | RMAN_register (IRESMAN_Fxns *resmanFxns, IRESMAN_Params *initArgs) |
| Register the IRESMAN protocol/protocol revision i.e., device specific resource manager implementation with the Resource Registry of RMAN. RMAN logs these entries in an internal table that is uses to satisfy requests for different IRES resources.
|
IRES_Status | RMAN_unregister (IRESMAN_Fxns *resmanFxns) |
| Unregisters the protocol and the corresponding resource manager implementation from RMAN's Resource Registry. This API is called when this resource no longer needs to be managed by RMAN.
|
IRES_Status | RMAN_assignResources (IALG_Handle algHandle, IRES_Fxns *resFxns, Int scratchGroupId) |
| Assign IRES resources to the algorithm indicated by algHandle. Algorithm could request multiple IRES resources of same/ different type through its IRES implementation. RMAN would identify which IRESMAN implementation (that is registered with it) to query and then request resources from that, to satisfy the individual IRES requests. Non-algorithm users of this API can obtain resources by passing * NULL as the algHandle. Resources will still be assigned to the IRES_Fxns::initResources API.
|
IRES_Status | RMAN_freeResources (IALG_Handle algHandle, IRES_Fxns *resFxns, Int scratchGroupId) |
| Free resources held by the algorithm resource handle.
|
IRES_Status | RMAN_activateResource (IALG_Handle algHandle, IRES_Handle resourceHandle, IRES_Fxns *resFxns, Int scratchGroupId) |
| Activate resource identified by the resourceHandle held by the algorithm.
|
IRES_Status | RMAN_activateAllResources (IALG_Handle algHandle, IRES_Fxns *resFxns, Int scratchGroupId) |
| Activate all resources held by the algorithm.
|
IRES_Status | RMAN_deactivateResource (IALG_Handle algHandle, IRES_Handle resourceHandle, IRES_Fxns *resFxns, Int scratchGroupId) |
| Deactivate resource identified by the resourceHandle held by the algorithm.
|
IRES_Status | RMAN_deactivateAllResources (IALG_Handle algHandle, IRES_Fxns *resFxns, Int scratchGroupId) |
| Deactivate all resources held by the algorithm.
|
void | RMAN_yield (IRES_YieldResourceType resource, IRES_YieldContextHandle algYieldContext, IRES_YieldArgs yieldArgs) |
| Yield function specifically for use when DSKT2 based algorithms need cooperative preemption and multi-tasking support This function is called by the algorithm at pre-determined points during its execution, to allow another algorithm of same, or higher prioirty to preempt its execution.
|
Variables |
__FAR__ RMAN_Params | RMAN_PARAMS |
__FAR__ IRESMAN_Fxns * | RMAN_TABLE [] |
__FAR__ short | RMAN_FREE_ENTRIES [] |
__FAR__ short | RMAN_numRegistryEntries |
__FAR__ IRESMAN_Fxns ** | RMAN_registryEntries |
__FAR__ IRESMAN_Params ** | RMAN_registryResmanArgs |