EDMA3_RM_GblErrCallbackParams Struct Reference
[EDMA3 Resource Manager Data Structures]

Global Error Callback parameters. More...

#include <edma3_rm.h>

Data Fields

EDMA3_RM_GblErrCallback gblerrCb
void * gblerrData

Detailed Description

Global Error Callback parameters.

Consists of the Callback function and the data to be passed to it.


Field Documentation

Instance wide callback function to catch non-channel specific errors.

Application data to be passed back to the Global Error callback


The documentation for this struct was generated from the following file:

Generated on Tue Dec 1 15:24:06 2009 for EDMA3 Resource Manager by  doxygen 1.6.1