EDMA3 Resource Manager Enums
[EDMA3 Resource Manager Symbols]

Enumerations

enum  EDMA3_RM_TccStatus {
  EDMA3_RM_XFER_COMPLETE = 1,
  EDMA3_RM_E_CC_DMA_EVT_MISS = 2,
  EDMA3_RM_E_CC_QDMA_EVT_MISS = 3
}
 

This enum defines the channel specific status codes of an EDMA3 transfer. It is returned while calling the channel specific callback function to tell the status.

More...
enum  EDMA3_RM_GlobalError {
  EDMA3_RM_E_CC_QUE_THRES_EXCEED = 1,
  EDMA3_RM_E_CC_TCC = 2,
  EDMA3_RM_E_TC_MEM_LOCATION_READ_ERROR = 3,
  EDMA3_RM_E_TC_MEM_LOCATION_WRITE_ERROR = 4,
  EDMA3_RM_E_TC_INVALID_ADDR = 5,
  EDMA3_RM_E_TC_TR_ERROR = 6
}
 

This enum defines the global (not specific to any channel) error codes of completion of an EDMA3 transfer.

More...
enum  EDMA3_RM_ResType {
  EDMA3_RM_RES_DMA_CHANNEL = 1,
  EDMA3_RM_RES_QDMA_CHANNEL = 2,
  EDMA3_RM_RES_TCC = 3,
  EDMA3_RM_RES_PARAM_SET = 4
}
 

EDMA3 Resource Type.

More...
enum  EDMA3_RM_HW_CHANNEL_EVENT {
  EDMA3_RM_HW_CHANNEL_EVENT_0 = 0,
  EDMA3_RM_HW_CHANNEL_EVENT_1,
  EDMA3_RM_HW_CHANNEL_EVENT_2,
  EDMA3_RM_HW_CHANNEL_EVENT_3,
  EDMA3_RM_HW_CHANNEL_EVENT_4,
  EDMA3_RM_HW_CHANNEL_EVENT_5,
  EDMA3_RM_HW_CHANNEL_EVENT_6,
  EDMA3_RM_HW_CHANNEL_EVENT_7,
  EDMA3_RM_HW_CHANNEL_EVENT_8,
  EDMA3_RM_HW_CHANNEL_EVENT_9,
  EDMA3_RM_HW_CHANNEL_EVENT_10,
  EDMA3_RM_HW_CHANNEL_EVENT_11,
  EDMA3_RM_HW_CHANNEL_EVENT_12,
  EDMA3_RM_HW_CHANNEL_EVENT_13,
  EDMA3_RM_HW_CHANNEL_EVENT_14,
  EDMA3_RM_HW_CHANNEL_EVENT_15,
  EDMA3_RM_HW_CHANNEL_EVENT_16,
  EDMA3_RM_HW_CHANNEL_EVENT_17,
  EDMA3_RM_HW_CHANNEL_EVENT_18,
  EDMA3_RM_HW_CHANNEL_EVENT_19,
  EDMA3_RM_HW_CHANNEL_EVENT_20,
  EDMA3_RM_HW_CHANNEL_EVENT_21,
  EDMA3_RM_HW_CHANNEL_EVENT_22,
  EDMA3_RM_HW_CHANNEL_EVENT_23,
  EDMA3_RM_HW_CHANNEL_EVENT_24,
  EDMA3_RM_HW_CHANNEL_EVENT_25,
  EDMA3_RM_HW_CHANNEL_EVENT_26,
  EDMA3_RM_HW_CHANNEL_EVENT_27,
  EDMA3_RM_HW_CHANNEL_EVENT_28,
  EDMA3_RM_HW_CHANNEL_EVENT_29,
  EDMA3_RM_HW_CHANNEL_EVENT_30,
  EDMA3_RM_HW_CHANNEL_EVENT_31,
  EDMA3_RM_HW_CHANNEL_EVENT_32,
  EDMA3_RM_HW_CHANNEL_EVENT_33,
  EDMA3_RM_HW_CHANNEL_EVENT_34,
  EDMA3_RM_HW_CHANNEL_EVENT_35,
  EDMA3_RM_HW_CHANNEL_EVENT_36,
  EDMA3_RM_HW_CHANNEL_EVENT_37,
  EDMA3_RM_HW_CHANNEL_EVENT_38,
  EDMA3_RM_HW_CHANNEL_EVENT_39,
  EDMA3_RM_HW_CHANNEL_EVENT_40,
  EDMA3_RM_HW_CHANNEL_EVENT_41,
  EDMA3_RM_HW_CHANNEL_EVENT_42,
  EDMA3_RM_HW_CHANNEL_EVENT_43,
  EDMA3_RM_HW_CHANNEL_EVENT_44,
  EDMA3_RM_HW_CHANNEL_EVENT_45,
  EDMA3_RM_HW_CHANNEL_EVENT_46,
  EDMA3_RM_HW_CHANNEL_EVENT_47,
  EDMA3_RM_HW_CHANNEL_EVENT_48,
  EDMA3_RM_HW_CHANNEL_EVENT_49,
  EDMA3_RM_HW_CHANNEL_EVENT_50,
  EDMA3_RM_HW_CHANNEL_EVENT_51,
  EDMA3_RM_HW_CHANNEL_EVENT_52,
  EDMA3_RM_HW_CHANNEL_EVENT_53,
  EDMA3_RM_HW_CHANNEL_EVENT_54,
  EDMA3_RM_HW_CHANNEL_EVENT_55,
  EDMA3_RM_HW_CHANNEL_EVENT_56,
  EDMA3_RM_HW_CHANNEL_EVENT_57,
  EDMA3_RM_HW_CHANNEL_EVENT_58,
  EDMA3_RM_HW_CHANNEL_EVENT_59,
  EDMA3_RM_HW_CHANNEL_EVENT_60,
  EDMA3_RM_HW_CHANNEL_EVENT_61,
  EDMA3_RM_HW_CHANNEL_EVENT_62,
  EDMA3_RM_HW_CHANNEL_EVENT_63
}
 

DMA Channels assigned to different Hardware Events.

More...
enum  EDMA3_RM_QdmaTrigWord {
  EDMA3_RM_QDMA_TRIG_OPT = 0,
  EDMA3_RM_QDMA_TRIG_SRC = 1,
  EDMA3_RM_QDMA_TRIG_ACNT_BCNT = 2,
  EDMA3_RM_QDMA_TRIG_DST = 3,
  EDMA3_RM_QDMA_TRIG_SRC_DST_BIDX = 4,
  EDMA3_RM_QDMA_TRIG_LINK_BCNTRLD = 5,
  EDMA3_RM_QDMA_TRIG_SRC_DST_CIDX = 6,
  EDMA3_RM_QDMA_TRIG_CCNT = 7,
  EDMA3_RM_QDMA_TRIG_DEFAULT = 7
}
 

QDMA Trigger Word.

More...
enum  EDMA3_RM_Cntrlr_PhyAddr {
  EDMA3_RM_CC_PHY_ADDR = 0,
  EDMA3_RM_TC0_PHY_ADDR,
  EDMA3_RM_TC1_PHY_ADDR,
  EDMA3_RM_TC2_PHY_ADDR,
  EDMA3_RM_TC3_PHY_ADDR,
  EDMA3_RM_TC4_PHY_ADDR,
  EDMA3_RM_TC5_PHY_ADDR,
  EDMA3_RM_TC6_PHY_ADDR,
  EDMA3_RM_TC7_PHY_ADDR
}
 

CC/TC Physical Address.

More...
enum  EDMA3_RM_IoctlCmd { ,
  EDMA3_RM_IOCTL_SET_PARAM_CLEAR_OPTION,
  EDMA3_RM_IOCTL_GET_PARAM_CLEAR_OPTION,
  EDMA3_RM_IOCTL_SET_GBL_REG_MODIFY_OPTION,
  EDMA3_RM_IOCTL_GET_GBL_REG_MODIFY_OPTION
}
 

EDMA3 Resource Manager IOCTL commands.

More...

Enumeration Type Documentation

This enum defines the channel specific status codes of an EDMA3 transfer. It is returned while calling the channel specific callback function to tell the status.

Enumerator:
EDMA3_RM_XFER_COMPLETE 

DMA Transfer successfully completed (true completion mode) or submitted to the TC (early completion mode).

EDMA3_RM_E_CC_DMA_EVT_MISS 

Channel Controller has reported an error DMA missed events:- for all 64 DMA channels. These get latched in the event missed registers (EMR/EMRH).

EDMA3_RM_E_CC_QDMA_EVT_MISS 

QDMA missed events:- for all QDMA channels. These get latched in the QDMA event missed register (QEMR).

This enum defines the global (not specific to any channel) error codes of completion of an EDMA3 transfer.

Enumerator:
EDMA3_RM_E_CC_QUE_THRES_EXCEED 

Threshold exceed:- for all event queues. These get latched in EDMA3CC error register (CCERR). This error has a direct relation with the setting of EDMA3_RM_GblConfigParams.evtQueueWaterMarkLvl

EDMA3_RM_E_CC_TCC 

TCC error:- for outstanding transfer requests expected to return completion code (TCCHEN or TCINTEN bit in OPT is set to 1) exceeding the maximum limit of 63. This also gets latched in the CCERR.

EDMA3_RM_E_TC_MEM_LOCATION_READ_ERROR 

Transfer Controller has reported an error Detection of a Read error signaled by the source or destination address

EDMA3_RM_E_TC_MEM_LOCATION_WRITE_ERROR 

Detection of a Write error signaled by the source or destination address

EDMA3_RM_E_TC_INVALID_ADDR 

Attempt to read or write to an invalid address in the configuration memory map.

EDMA3_RM_E_TC_TR_ERROR 

Detection of a FIFO mode TR violating the FIFO mode transfer rules (the source/destination addresses and source/destination indexes must be aligned to 32 bytes).

EDMA3 Resource Type.

Enumerator:
EDMA3_RM_RES_DMA_CHANNEL 

DMA Channel resource

EDMA3_RM_RES_QDMA_CHANNEL 

QDMA Channel resource

EDMA3_RM_RES_TCC 

TCC resource

EDMA3_RM_RES_PARAM_SET 

Parameter RAM Set resource

DMA Channels assigned to different Hardware Events.

They should be used while requesting a specific DMA channel. One possible usage is to maintain a SoC specific file, which will contain the mapping of these hardware events to the respective peripherals for better understanding and lesser probability of errors. Also, if any event associated with a particular peripheral gets changed, only that SoC specific file needs to be changed. for eg, the sample SoC specific file "soc.h" can have these defines:

define EDMA3_RM_HW_CHANNEL_MCBSP_TX EDMA3_RM_HW_CHANNEL_EVENT_2 define EDMA3_RM_HW_CHANNEL_MCBSP_RX EDMA3_RM_HW_CHANNEL_EVENT_3

These defines will be used by the MCBSP driver. The same event EDMA3_RM_HW_CHANNEL_EVENT_2/3 could be mapped to some other peripheral also.

Enumerator:
EDMA3_RM_HW_CHANNEL_EVENT_0 

Channel assigned to EDMA3 Event 0

EDMA3_RM_HW_CHANNEL_EVENT_1 

Channel assigned to EDMA3 Event 1

EDMA3_RM_HW_CHANNEL_EVENT_2 

Channel assigned to EDMA3 Event 2

EDMA3_RM_HW_CHANNEL_EVENT_3 

Channel assigned to EDMA3 Event 3

EDMA3_RM_HW_CHANNEL_EVENT_4 

Channel assigned to EDMA3 Event 4

EDMA3_RM_HW_CHANNEL_EVENT_5 

Channel assigned to EDMA3 Event 5

EDMA3_RM_HW_CHANNEL_EVENT_6 

Channel assigned to EDMA3 Event 6

EDMA3_RM_HW_CHANNEL_EVENT_7 

Channel assigned to EDMA3 Event 7

EDMA3_RM_HW_CHANNEL_EVENT_8 

Channel assigned to EDMA3 Event 8

EDMA3_RM_HW_CHANNEL_EVENT_9 

Channel assigned to EDMA3 Event 9

EDMA3_RM_HW_CHANNEL_EVENT_10 

Channel assigned to EDMA3 Event 10

EDMA3_RM_HW_CHANNEL_EVENT_11 

Channel assigned to EDMA3 Event 11

EDMA3_RM_HW_CHANNEL_EVENT_12 

Channel assigned to EDMA3 Event 12

EDMA3_RM_HW_CHANNEL_EVENT_13 

Channel assigned to EDMA3 Event 13

EDMA3_RM_HW_CHANNEL_EVENT_14 

Channel assigned to EDMA3 Event 14

EDMA3_RM_HW_CHANNEL_EVENT_15 

Channel assigned to EDMA3 Event 15

EDMA3_RM_HW_CHANNEL_EVENT_16 

Channel assigned to EDMA3 Event 16

EDMA3_RM_HW_CHANNEL_EVENT_17 

Channel assigned to EDMA3 Event 17

EDMA3_RM_HW_CHANNEL_EVENT_18 

Channel assigned to EDMA3 Event 18

EDMA3_RM_HW_CHANNEL_EVENT_19 

Channel assigned to EDMA3 Event 19

EDMA3_RM_HW_CHANNEL_EVENT_20 

Channel assigned to EDMA3 Event 20

EDMA3_RM_HW_CHANNEL_EVENT_21 

Channel assigned to EDMA3 Event 21

EDMA3_RM_HW_CHANNEL_EVENT_22 

Channel assigned to EDMA3 Event 22

EDMA3_RM_HW_CHANNEL_EVENT_23 

Channel assigned to EDMA3 Event 23

EDMA3_RM_HW_CHANNEL_EVENT_24 

Channel assigned to EDMA3 Event 24

EDMA3_RM_HW_CHANNEL_EVENT_25 

Channel assigned to EDMA3 Event 25

EDMA3_RM_HW_CHANNEL_EVENT_26 

Channel assigned to EDMA3 Event 26

EDMA3_RM_HW_CHANNEL_EVENT_27 

Channel assigned to EDMA3 Event 27

EDMA3_RM_HW_CHANNEL_EVENT_28 

Channel assigned to EDMA3 Event 28

EDMA3_RM_HW_CHANNEL_EVENT_29 

Channel assigned to EDMA3 Event 29

EDMA3_RM_HW_CHANNEL_EVENT_30 

Channel assigned to EDMA3 Event 30

EDMA3_RM_HW_CHANNEL_EVENT_31 

Channel assigned to EDMA3 Event 31

EDMA3_RM_HW_CHANNEL_EVENT_32 

Channel assigned to EDMA3 Event 32

EDMA3_RM_HW_CHANNEL_EVENT_33 

Channel assigned to EDMA3 Event 33

EDMA3_RM_HW_CHANNEL_EVENT_34 

Channel assigned to EDMA3 Event 34

EDMA3_RM_HW_CHANNEL_EVENT_35 

Channel assigned to EDMA3 Event 35

EDMA3_RM_HW_CHANNEL_EVENT_36 

Channel assigned to EDMA3 Event 36

EDMA3_RM_HW_CHANNEL_EVENT_37 

Channel assigned to EDMA3 Event 37

EDMA3_RM_HW_CHANNEL_EVENT_38 

Channel assigned to EDMA3 Event 38

EDMA3_RM_HW_CHANNEL_EVENT_39 

Channel assigned to EDMA3 Event 39

EDMA3_RM_HW_CHANNEL_EVENT_40 

Channel assigned to EDMA3 Event 40

EDMA3_RM_HW_CHANNEL_EVENT_41 

Channel assigned to EDMA3 Event 41

EDMA3_RM_HW_CHANNEL_EVENT_42 

Channel assigned to EDMA3 Event 42

EDMA3_RM_HW_CHANNEL_EVENT_43 

Channel assigned to EDMA3 Event 43

EDMA3_RM_HW_CHANNEL_EVENT_44 

Channel assigned to EDMA3 Event 44

EDMA3_RM_HW_CHANNEL_EVENT_45 

Channel assigned to EDMA3 Event 45

EDMA3_RM_HW_CHANNEL_EVENT_46 

Channel assigned to EDMA3 Event 46

EDMA3_RM_HW_CHANNEL_EVENT_47 

Channel assigned to EDMA3 Event 47

EDMA3_RM_HW_CHANNEL_EVENT_48 

Channel assigned to EDMA3 Event 48

EDMA3_RM_HW_CHANNEL_EVENT_49 

Channel assigned to EDMA3 Event 49

EDMA3_RM_HW_CHANNEL_EVENT_50 

Channel assigned to EDMA3 Event 50

EDMA3_RM_HW_CHANNEL_EVENT_51 

Channel assigned to EDMA3 Event 51

EDMA3_RM_HW_CHANNEL_EVENT_52 

Channel assigned to EDMA3 Event 52

EDMA3_RM_HW_CHANNEL_EVENT_53 

Channel assigned to EDMA3 Event 53

EDMA3_RM_HW_CHANNEL_EVENT_54 

Channel assigned to EDMA3 Event 54

EDMA3_RM_HW_CHANNEL_EVENT_55 

Channel assigned to EDMA3 Event 55

EDMA3_RM_HW_CHANNEL_EVENT_56 

Channel assigned to EDMA3 Event 56

EDMA3_RM_HW_CHANNEL_EVENT_57 

Channel assigned to EDMA3 Event 57

EDMA3_RM_HW_CHANNEL_EVENT_58 

Channel assigned to EDMA3 Event 58

EDMA3_RM_HW_CHANNEL_EVENT_59 

Channel assigned to EDMA3 Event 59

EDMA3_RM_HW_CHANNEL_EVENT_60 

Channel assigned to EDMA3 Event 60

EDMA3_RM_HW_CHANNEL_EVENT_61 

Channel assigned to EDMA3 Event 61

EDMA3_RM_HW_CHANNEL_EVENT_62 

Channel assigned to EDMA3 Event 62

EDMA3_RM_HW_CHANNEL_EVENT_63 

Channel assigned to EDMA3 Event 63

QDMA Trigger Word.

Use this enum to set the QDMA trigger word to any of the 8 DWords(unsigned int) within a Parameter RAM set

Enumerator:
EDMA3_RM_QDMA_TRIG_OPT 

Set the OPT field (Offset Address 0h Bytes) as the QDMA trigger word

EDMA3_RM_QDMA_TRIG_SRC 

Set the SRC field (Offset Address 4h Bytes) as the QDMA trigger word

EDMA3_RM_QDMA_TRIG_ACNT_BCNT 

Set the (ACNT + BCNT) field (Offset Address 8h Bytes) as the QDMA trigger word

EDMA3_RM_QDMA_TRIG_DST 

Set the DST field (Offset Address Ch Bytes) as the QDMA trigger word

EDMA3_RM_QDMA_TRIG_SRC_DST_BIDX 

Set the (SRCBIDX + DSTBIDX) field (Offset Address 10h Bytes) as the QDMA trigger word

EDMA3_RM_QDMA_TRIG_LINK_BCNTRLD 

Set the (LINK + BCNTRLD) field (Offset Address 14h Bytes) as the QDMA trigger word

EDMA3_RM_QDMA_TRIG_SRC_DST_CIDX 

Set the (SRCCIDX + DSTCIDX) field (Offset Address 18h Bytes) as the QDMA trigger word

EDMA3_RM_QDMA_TRIG_CCNT 

Set the (CCNT + RSVD) field (Offset Address 1Ch Bytes) as the QDMA trigger word

EDMA3_RM_QDMA_TRIG_DEFAULT 

Default Trigger Word

CC/TC Physical Address.

Use this enum to get the physical address of the Channel Controller or the Transfer Controller. The address returned could be used by the advanced users to set/get some specific registers direclty.

Enumerator:
EDMA3_RM_CC_PHY_ADDR 

Channel Controller Physical Address

EDMA3_RM_TC0_PHY_ADDR 

Transfer Controller 0 Physical Address

EDMA3_RM_TC1_PHY_ADDR 

Transfer Controller 1 Physical Address

EDMA3_RM_TC2_PHY_ADDR 

Transfer Controller 2 Physical Address

EDMA3_RM_TC3_PHY_ADDR 

Transfer Controller 3 Physical Address

EDMA3_RM_TC4_PHY_ADDR 

Transfer Controller 4 Physical Address

EDMA3_RM_TC5_PHY_ADDR 

Transfer Controller 5 Physical Address

EDMA3_RM_TC6_PHY_ADDR 

Transfer Controller 6 Physical Address

EDMA3_RM_TC7_PHY_ADDR 

Transfer Controller 7 Physical Address

EDMA3 Resource Manager IOCTL commands.

Enumerator:
EDMA3_RM_IOCTL_SET_PARAM_CLEAR_OPTION 

PaRAM Sets will be cleared OR will not be cleared during allocation, depending upon this option.

For e.g., To clear the PaRAM Sets during allocation, cmdArg = (void *)1;

To NOT clear the PaRAM Sets during allocation, cmdArg = (void *)0;

For all other values, it will return error.

By default, PaRAM Sets will be cleared during allocation.

Note: Since this enum can change the behavior how the resources are initialized during their allocation, user is adviced to not use this command while allocating the resources. User should first change the behavior of resources' initialization and then should use start allocating resources.

EDMA3_RM_IOCTL_GET_PARAM_CLEAR_OPTION 

To check whether PaRAM Sets will be cleared or not during allocation. If the value read is '1', it means that PaRAM Sets are getting cleared during allocation. If the value read is '0', it means that PaRAM Sets are NOT getting cleared during allocation.

For e.g., unsigned int *isParamClearingDone = (unsigned int *)cmdArg; (*isParamClearingDone) = paramClearingRequired;

EDMA3_RM_IOCTL_SET_GBL_REG_MODIFY_OPTION 

Global EDMA3 registers (DCHMAP/QCHMAP) and PaRAM Sets will be modified OR will not be modified during EDMA3_RM_allocLogicalChannel (), depending upon this option.

For e.g., To modify the Registers or PaRAM Sets during allocation, cmdArg = (void *)1;

To NOT modify the Registers or PaRAM Sets during allocation, cmdArg = (void *)0;

For all other values, it will return error.

By default, Registers or PaRAM Sets will be programmed during allocation.

Note: Since this enum can change the behavior how the resources are initialized during their allocation, user is adviced to not use this command while allocating the resources. User should first change the behavior of resources' initialization and then should use start allocating resources.

EDMA3_RM_IOCTL_GET_GBL_REG_MODIFY_OPTION 

To check whether Global EDMA3 registers (DCHMAP/QCHMAP) and PaRAM Sets will be programmed or not during allocation (EDMA3_RM_allocLogicalChannel ()). If the value read is '1', it means that the registers/PaRAMs are getting programmed during allocation. If the value read is '0', it means that the registers/PaRAMs are NOT getting programmed during allocation.

For e.g., unsigned int *isParamClearingDone = (unsigned int *)cmdArg; (*isParamClearingDone) = paramClearingRequired;


Generated on Tue Dec 1 15:24:04 2009 for EDMA3 Resource Manager by  doxygen 1.6.1