EDMA3 Resource Manager Defines
[EDMA3 Resource Manager Symbols]

Defines

#define EDMA3_RM_RES_ANY   (1010u)
 Used to specify any available Resource Id (EDMA3_RM_ResDesc.resId).
#define EDMA3_RM_E_BASE   (-155)
#define EDMA3_RM_E_OBJ_NOT_DELETED   (EDMA3_RM_E_BASE)
#define EDMA3_RM_E_OBJ_NOT_CLOSED   (EDMA3_RM_E_BASE-1)
#define EDMA3_RM_E_OBJ_NOT_OPENED   (EDMA3_RM_E_BASE-2)
#define EDMA3_RM_E_INVALID_PARAM   (EDMA3_RM_E_BASE-3)
#define EDMA3_RM_E_RES_ALREADY_FREE   (EDMA3_RM_E_BASE-4)
#define EDMA3_RM_E_RES_NOT_OWNED   (EDMA3_RM_E_BASE-5)
#define EDMA3_RM_E_SPECIFIED_RES_NOT_AVAILABLE   (EDMA3_RM_E_BASE-6)
#define EDMA3_RM_E_ALL_RES_NOT_AVAILABLE   (EDMA3_RM_E_BASE-7)
#define EDMA3_RM_E_INVALID_STATE   (EDMA3_RM_E_BASE-8)
#define EDMA3_RM_E_MAX_RM_INST_OPENED   (EDMA3_RM_E_BASE-9)
#define EDMA3_RM_E_RM_MASTER_ALREADY_EXISTS   (EDMA3_RM_E_BASE-10)
#define EDMA3_RM_E_CALLBACK_ALREADY_REGISTERED   (EDMA3_RM_E_BASE-11)
#define EDMA3_RM_E_SEMAPHORE   (EDMA3_RM_E_BASE-12)
#define EDMA3_RM_E_FEATURE_UNSUPPORTED   (EDMA3_RM_E_BASE-13)
#define EDMA3_RM_E_RES_NOT_ALLOCATED   (EDMA3_RM_E_BASE-14)
#define EDMA3_RM_DMA_CHANNEL_ANY   (1011u)
#define EDMA3_RM_QDMA_CHANNEL_ANY   (1012u)
#define EDMA3_RM_TCC_ANY   (1013u)
#define EDMA3_RM_PARAM_ANY   (1014u)
#define EDMA3_RM_CH_NO_PARAM_MAP   (1015u)
#define EDMA3_RM_CH_NO_TCC_MAP   (1016u)

Define Documentation

#define EDMA3_RM_E_BASE   (-155)

Resource Manager Error Codes base define

#define EDMA3_RM_E_OBJ_NOT_DELETED   (EDMA3_RM_E_BASE)

Resource Manager Object Not Deleted yet. So the object cannot be created.

#define EDMA3_RM_E_OBJ_NOT_CLOSED   (EDMA3_RM_E_BASE-1)

Resource Manager Object Not Closed yet. So the object cannot be deleted.

#define EDMA3_RM_E_OBJ_NOT_OPENED   (EDMA3_RM_E_BASE-2)

Resource Manager Object Not Opened yet So the object cannot be closed.

#define EDMA3_RM_E_INVALID_PARAM   (EDMA3_RM_E_BASE-3)

Invalid Parameter passed to API

#define EDMA3_RM_E_RES_ALREADY_FREE   (EDMA3_RM_E_BASE-4)

Resource requested for freeing is already free

#define EDMA3_RM_E_RES_NOT_OWNED   (EDMA3_RM_E_BASE-5)

Resource requested for allocation/freeing is not owned

#define EDMA3_RM_E_SPECIFIED_RES_NOT_AVAILABLE   (EDMA3_RM_E_BASE-6)

Resource is not available

#define EDMA3_RM_E_ALL_RES_NOT_AVAILABLE   (EDMA3_RM_E_BASE-7)

No Resource of specified type is available

#define EDMA3_RM_E_INVALID_STATE   (EDMA3_RM_E_BASE-8)

Invalid State of EDMA3 RM Obj

#define EDMA3_RM_E_MAX_RM_INST_OPENED   (EDMA3_RM_E_BASE-9)

Maximum no of Res Mgr Instances already Opened

#define EDMA3_RM_E_RM_MASTER_ALREADY_EXISTS   (EDMA3_RM_E_BASE-10)

More than one Res Mgr Master Instance NOT supported. Only 1 master can exist.

#define EDMA3_RM_E_CALLBACK_ALREADY_REGISTERED   (EDMA3_RM_E_BASE-11)

Callback function already registered.

#define EDMA3_RM_E_SEMAPHORE   (EDMA3_RM_E_BASE-12)

Semaphore related error

#define EDMA3_RM_E_FEATURE_UNSUPPORTED   (EDMA3_RM_E_BASE-13)

Hardware feature NOT supported

#define EDMA3_RM_E_RES_NOT_ALLOCATED   (EDMA3_RM_E_BASE-14)

EDMA3 Resource NOT allocated

#define EDMA3_RM_DMA_CHANNEL_ANY   (1011u)

Used to specify any available DMA Channel while requesting one. Used in the API EDMA3_RM_allocLogicalChannel (). DMA channel from the pool of (owned && non_reserved && available_right_now) DMA channels will be chosen and returned.

#define EDMA3_RM_QDMA_CHANNEL_ANY   (1012u)

Used to specify any available QDMA Channel while requesting one. Used in the API EDMA3_RM_allocLogicalChannel(). QDMA channel from the pool of (owned && non_reserved && available_right_now) QDMA channels will be chosen and returned.

#define EDMA3_RM_TCC_ANY   (1013u)

Used to specify any available TCC while requesting one. Used in the API EDMA3_RM_allocLogicalChannel(), for both DMA and QDMA channels. TCC from the pool of (owned && non_reserved && available_right_now) TCCs will be chosen and returned.

#define EDMA3_RM_PARAM_ANY   (1014u)

Used to specify any available PaRAM Set while requesting one. Used in the API EDMA3_RM_allocLogicalChannel(), for both DMA/QDMA and Link channels. PaRAM Set from the pool of (owned && non_reserved && available_right_now) PaRAM Sets will be chosen and returned.

#define EDMA3_RM_CH_NO_PARAM_MAP   (1015u)

This define is used to specify that a DMA channel is NOT tied to any PaRAM Set and hence any available PaRAM Set could be used for that DMA channel. It could be used in dmaChannelPaRAMMap [EDMA3_MAX_DMA_CH], in global configuration structure EDMA3_RM_GblConfigParams.

This value should mandatorily be used to mark DMA channels with no initial mapping to specific PaRAM Sets.

#define EDMA3_RM_CH_NO_TCC_MAP   (1016u)

This define is used to specify that the DMA/QDMA channel is not tied to any TCC and hence any available TCC could be used for that DMA/QDMA channel. It could be used in dmaChannelTccMap [EDMA3_MAX_DMA_CH], in global configuration structure EDMA3_RM_GblConfigParams.

This value should mandatorily be used to mark DMA channels with no initial mapping to specific TCCs.


Generated on Tue Dec 1 15:24:04 2009 for EDMA3 Resource Manager by  doxygen 1.6.1