EDMA3_DRV_ParamentryRegs Struct Reference
[EDMA3 Driver Data Structures]

EDMA3 PaRAM Set. More...

#include <edma3_drv.h>

Data Fields

volatile unsigned int OPT
volatile unsigned int SRC
 Starting byte address of Source For FIFO mode, srcAddr must be a 256-bit aligned address.
volatile unsigned int A_B_CNT
volatile unsigned int DST
 Starting byte address of destination For FIFO mode, destAddr must be a 256-bit aligned address. i.e. 5 LSBs should be 0.
volatile unsigned int SRC_DST_BIDX
volatile unsigned int LINK_BCNTRLD
 Address for linking (AutoReloading of a PaRAM Set) (16 bits) and Reload value of the numArrInFrame (BCNT) (16 bits).
volatile unsigned int SRC_DST_CIDX
 Index between consecutive frames of a Source Block (SRCCIDX) (16 bits) and Index between consecutive frames of a Dest Block (DSTCIDX) (16 bits).
volatile unsigned int CCNT
 Number of Frames in a block (CCNT) (16 bits).

Detailed Description

EDMA3 PaRAM Set.

This is a mapping of the EDMA3 PaRAM set provided to the user for ease of modification of the individual PaRAM words.


Field Documentation

volatile unsigned int EDMA3_DRV_ParamentryRegs::OPT

OPT field of PaRAM Set

volatile unsigned int EDMA3_DRV_ParamentryRegs::A_B_CNT

Number of bytes in each Array (ACNT) (16 bits) and Number of Arrays in each Frame (BCNT) (16 bits).

Index between consec. arrays of a Source Frame (SRCBIDX) (16 bits) and Index between consec. arrays of a Destination Frame (DSTBIDX) (16 bits).

If SAM is set to 1 (via channelOptions) then srcInterArrIndex should be an even multiple of 32 bytes.

If DAM is set to 1 (via channelOptions) then destInterArrIndex should be an even multiple of 32 bytes

Address for linking (AutoReloading of a PaRAM Set) (16 bits) and Reload value of the numArrInFrame (BCNT) (16 bits).

Link field must point to a valid aligned 32-byte PaRAM set A value of 0xFFFF means no linking.

B count reload field is relevant only for A-sync transfers.


The documentation for this struct was generated from the following file:

Generated on Tue Dec 1 15:12:10 2009 for EDMA3 Driver by  doxygen 1.6.1