EDMA3_DRV_ChBoundResources Struct Reference

EDMA3 Channel-Bound resources. More...

#include <edma3.h>

Data Fields

int paRAMId
unsigned int tcc
EDMA3_DRV_TrigMode trigMode

Detailed Description

EDMA3 Channel-Bound resources.

Used to maintain information of the EDMA3 resources (specifically Parameter RAM set and TCC) and the mode of triggering transfer (Manual, HW event driven etc) bound to the particular channel within EDMA3_DRV_requestChannel().


Field Documentation

PaRAM Set number associated with the particular channel

TCC associated with the particular channel

Mode of triggering transfer


The documentation for this struct was generated from the following file:

Generated on Tue Dec 1 15:12:10 2009 for EDMA3 Driver by  doxygen 1.6.1