EDMA3_RM_MiscParam Struct Reference
[Interface Definition for EDMA3 Resource Manager Layer]

Used to specify the miscellaneous options during Resource Manager Initialization. More...

#include <edma3_rm.h>


Data Fields

unsigned short isSlave
unsigned short param


Detailed Description

Used to specify the miscellaneous options during Resource Manager Initialization.

This configuration structure is used to specify some misc options while creating the RM Object. New options may also be added into this structure in future.


Field Documentation

In a multi-master system (for e.g. ARM + DSP), this option is used to distinguish between Master and Slave. Only the Master is allowed to program the global EDMA3 registers (like Queue priority, Queue water- mark level, error registers etc).

Referenced by EDMA3_RM_create().

unsigned short EDMA3_RM_MiscParam::param

For future use


The documentation for this struct was generated from the following file:

Generated on Tue Jul 7 19:26:49 2009 for EDMA3 Resource Manager by  doxygen 1.5.9