#include <edma3_drv.h>
Data Fields | |
volatile unsigned int | OPT |
volatile unsigned int | SRC |
Starting byte address of Source For FIFO mode, srcAddr must be a 256-bit aligned address. | |
volatile unsigned int | A_B_CNT |
volatile unsigned int | DST |
Starting byte address of destination For FIFO mode, destAddr must be a 256-bit aligned address. i.e. 5 LSBs should be 0. | |
volatile unsigned int | SRC_DST_BIDX |
volatile unsigned int | LINK_BCNTRLD |
Address for linking (AutoReloading of a PaRAM Set) (16 bits) and Reload value of the numArrInFrame (BCNT) (16 bits). | |
volatile unsigned int | SRC_DST_CIDX |
Index between consecutive frames of a Source Block (SRCCIDX) (16 bits) and Index between consecutive frames of a Dest Block (DSTCIDX) (16 bits). | |
volatile unsigned int | CCNT |
Number of Frames in a block (CCNT) (16 bits). |
This is a mapping of the EDMA3 PaRAM set provided to the user for ease of modification of the individual PaRAM words.
volatile unsigned int EDMA3_DRV_ParamentryRegs::A_B_CNT |
Number of bytes in each Array (ACNT) (16 bits) and Number of Arrays in each Frame (BCNT) (16 bits).
volatile unsigned int EDMA3_DRV_ParamentryRegs::LINK_BCNTRLD |
Address for linking (AutoReloading of a PaRAM Set) (16 bits) and Reload value of the numArrInFrame (BCNT) (16 bits).
Link field must point to a valid aligned 32-byte PaRAM set A value of 0xFFFF means no linking.
B count reload field is relevant only for A-sync transfers.
volatile unsigned int EDMA3_DRV_ParamentryRegs::OPT |
OPT field of PaRAM Set
volatile unsigned int EDMA3_DRV_ParamentryRegs::SRC_DST_BIDX |
Index between consec. arrays of a Source Frame (SRCBIDX) (16 bits) and Index between consec. arrays of a Destination Frame (DSTBIDX) (16 bits).
If SAM is set to 1 (via channelOptions) then srcInterArrIndex should be an even multiple of 32 bytes.
If DAM is set to 1 (via channelOptions) then destInterArrIndex should be an even multiple of 32 bytes