![]() |
![]() |
Defines the run time output arguments for all IVIDENC1 instance objects. More...
#include <ividenc1.h>
Defines the run time output arguments for all IVIDENC1 instance objects.
size
parameter. size
field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details.Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
Extended error information.
Number of bytes generated during the IVIDENC1_Fxns::process() call.
Video frame types.
IVIDEO_xy_FRAME
values, this frame type is interlaced where both top and bottom fields are provided in a single frame. The first field is an "x" frame, the second field is "y" field.Video frame skipping modes.
Output ID corresponding with the encoded buffer. This shall also be used to free up the corresponding image buffer for further use by client application code.
The encoder fills the buffer with the encoded bitstream. In case of sequences having I & P frames only, these values are identical to outBufs
passed in IVIDENC1_Fxns::process().
encodedBuf.bufSize
field returned corresponds to the actual valid size of the memory buffer. See the bytesGenerated
field for how much data is in this buffer.outputID
and encodedBuf
together provide info relating to the corresponding encoded image buffer. Reconstruction frames.
outBufs->bufs
[1], outBufs->bufs
[2], and outBufs->bufs
[3].reconBufs.bufDesc
[0].buf is equivalent to outBufs->bufs
[1], reconBufs.bufDesc
[1].buf is equivalent to outBufs->bufs
[2], and reconBufs.bufDesc
[2].buf is equivalent to outBufs->bufs
[3].