Defines the creation time parameters for all IVIDANALYTICS instance objects. More...
#include <ividanalytics.h>
Data Fields | |
XDAS_Int32 | size |
XDAS_Int32 | maxHeight |
XDAS_Int32 | maxWidth |
XDAS_Int32 | maxFrameRate |
XDAS_Int32 | dataEndianness |
XDAS_Int32 | inputChromaFormat |
XDAS_Int32 | maxRules |
Defines the creation time parameters for all IVIDANALYTICS instance objects.
size
parameter. size
field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details. Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
Maximum video height in pixels.
Maximum video width in pixels.
Maximum frame rate in fps * 1000. For example, if max frame rate is 30 frames per second, set this field to 30000.
Endianness of output data.
Chroma format for the input buffer.
Maximum number of rules allowed.