![]() |
![]() |
Defines the creation time parameters for all IIMGENC instance objects. More...
#include <iimgenc.h>
Data Fields | |
XDAS_Int32 | size |
XDAS_Int32 | maxHeight |
XDAS_Int32 | maxWidth |
XDAS_Int32 | maxScans |
XDAS_Int32 | dataEndianness |
XDAS_Int32 | forceChromaFormat |
Defines the creation time parameters for all IIMGENC instance objects.
size
parameter. size
field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details. Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
Maximum height.
Maximum width.
Maximum number of scans.
Endianness of output data.
Force encoding in given Chroma format.