![]() |
![]() |
Defines the input arguments for all IAUDENC1 instance process function. More...
#include <iaudenc1.h>
Data Fields | |
XDAS_Int32 | size |
XDAS_Int32 | numInSamples |
XDM1_SingleBufDesc | ancData |
Defines the input arguments for all IAUDENC1 instance process function.
size
parameter. size
field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details.Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
Number of Input Samples per Channel.
Ancillary Data.