![]() |
![]() |
This structure defines the algorithm parameters that can be modified after creation via control() calls. More...
#include <iaudenc1.h>
Data Fields | |
XDAS_Int32 | size |
XDAS_Int32 | bitRate |
XDAS_Int32 | sampleRate |
XDAS_Int32 | channelMode |
XDAS_Int32 | lfeFlag |
XDAS_Int32 | dualMonoMode |
XDAS_Int32 | inputBitsPerSample |
This structure defines the algorithm parameters that can be modified after creation via control() calls.
size
parameter. size
field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details.Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
Average bit rate, in bits per second.
Sampling frequency in Hz. For example, if the sampling frequency is 44.1 kHz, this field will be 44100.
Input Channel Mode.
Flag indicating whether LFE channel data is present or not in the input.
Valid values for this field are XDAS_TRUE and XDAS_FALSE.
Mode to indicate type of Dual Mono. Applicable only if channelMode is dualMono
Number of input bits per output sample. For example, if there are 16 bits per PCM input sample, this should be set to 16.