Data Structures | |
struct | IIMGDEC1_Obj |
This must be the first field of all IIMGDEC1 instance objects. More... | |
struct | IIMGDEC1_Params |
Defines the creation time parameters for all IIMGDEC1 instance objects. More... | |
struct | IIMGDEC1_DynamicParams |
This structure defines the codec parameters that can be modified after creation via control() calls. More... | |
struct | IIMGDEC1_InArgs |
Defines the input arguments for all IIMGDEC1 instance process() function. More... | |
struct | IIMGDEC1_Status |
Defines instance status parameters. More... | |
struct | IIMGDEC1_OutArgs |
Defines the run time output arguments for all IIMGDEC1 instance objects. More... | |
struct | IIMGDEC1_Fxns |
Defines all of the operations on IIMGDEC1 objects. More... | |
Defines | |
#define | IIMGDEC1_EOK XDM_EOK |
#define | IIMGDEC1_EFAIL XDM_EFAIL |
#define | IIMGDEC1_EUNSUPPORTED XDM_EUNSUPPORTED |
Typedefs | |
typedef struct IIMGDEC1_Obj | IIMGDEC1_Obj |
This must be the first field of all IIMGDEC1 instance objects. | |
typedef struct IIMGDEC1_Obj * | IIMGDEC1_Handle |
Opaque handle to an IIMGDEC1 objects. | |
typedef struct IIMGDEC1_Params | IIMGDEC1_Params |
Defines the creation time parameters for all IIMGDEC1 instance objects. | |
typedef struct IIMGDEC1_DynamicParams | IIMGDEC1_DynamicParams |
This structure defines the codec parameters that can be modified after creation via control() calls. | |
typedef struct IIMGDEC1_InArgs | IIMGDEC1_InArgs |
Defines the input arguments for all IIMGDEC1 instance process() function. | |
typedef struct IIMGDEC1_Status | IIMGDEC1_Status |
Defines instance status parameters. | |
typedef struct IIMGDEC1_OutArgs | IIMGDEC1_OutArgs |
Defines the run time output arguments for all IIMGDEC1 instance objects. | |
typedef IALG_Cmd | IIMGDEC1_Cmd |
Defines the control commands for the IIMGDEC1 module. | |
typedef struct IIMGDEC1_Fxns | IIMGDEC1_Fxns |
Defines all of the operations on IIMGDEC1 objects. |
This is the XDM IIMGDEC1 Image Decoder Interface.
#define IIMGDEC1_EOK XDM_EOK |
Success.
#define IIMGDEC1_EFAIL XDM_EFAIL |
General failure.
#define IIMGDEC1_EUNSUPPORTED XDM_EUNSUPPORTED |
Request is unsupported.
typedef struct IIMGDEC1_Obj IIMGDEC1_Obj |
This must be the first field of all IIMGDEC1 instance objects.
typedef struct IIMGDEC1_Obj* IIMGDEC1_Handle |
Opaque handle to an IIMGDEC1 objects.
typedef struct IIMGDEC1_Params IIMGDEC1_Params |
Defines the creation time parameters for all IIMGDEC1 instance objects.
size
parameter. size
field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details. typedef struct IIMGDEC1_DynamicParams IIMGDEC1_DynamicParams |
This structure defines the codec parameters that can be modified after creation via control() calls.
size
parameter. size
field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details.typedef struct IIMGDEC1_InArgs IIMGDEC1_InArgs |
Defines the input arguments for all IIMGDEC1 instance process() function.
size
parameter. size
field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details.typedef struct IIMGDEC1_Status IIMGDEC1_Status |
Defines instance status parameters.
size
parameter. size
field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details.typedef struct IIMGDEC1_OutArgs IIMGDEC1_OutArgs |
Defines the run time output arguments for all IIMGDEC1 instance objects.
size
parameter. size
field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details.typedef IALG_Cmd IIMGDEC1_Cmd |
Defines the control commands for the IIMGDEC1 module.
typedef struct IIMGDEC1_Fxns IIMGDEC1_Fxns |
Defines all of the operations on IIMGDEC1 objects.