![]() |
![]() |
This structure is passed to Engine_add()
, and contains parameters to specify an engine.
More...
#include <Engine.h>
Data Fields | |
String | name |
Engine_AlgDesc * | algTab |
String | remoteName |
String | memMap |
Bool | useExtLoader |
Int | numAlgs |
Int | heapId |
This structure is passed to Engine_add()
, and contains parameters to specify an engine.
String Engine_Desc::name |
Name of the Engine
No longer used, set to NULL
String Engine_Desc::remoteName |
Name of Server image, if applicable
String Engine_Desc::memMap |
Name of a file containing the slave memory map
Indicates whether the Server containing any remote algorithms will be loaded using an external loader (e.g. SysLink's slaveloader)
useExtLoader
is TRUE, Engine_open() will not load the slave.useExtLoader
is FALSE, Engine_open() will load the Server with the file specified by remoteName
. No longer used, set to zero
No longer used, set to zero