![]() |
![]() |
This structure defines the algorithm parameters that can be modified after creation via IVIDDEC3_Fxns.control() calls. More...
#include <ividdec3.h>
This structure defines the algorithm parameters that can be modified after creation via IVIDDEC3_Fxns.control() calls.
size
parameter. size
field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
Decode entire access unit or only header.
Pitch. If set to zero, use the decoded image width. Else, use given display width in pixels. Display width has to be greater than or equal to image width.
Video frame skip features for video decoder.
Flag to indicate that the algorithm should start a new frame.
Optional datasync "put data" function.
Datasync "put data" handle
Datasync "get data" function.
Datasync "get data" handle
getDataFxn
.Datasync "put buffer" function.
Datasync "put buffer" handle
Argument used during late acquire.
lateAcquireArg
value when requesting resources (i.e. during their call to acquire() when requesting the resource).