Defines |
#define | AUDENC1_EOK IAUDENC1_EOK |
#define | AUDENC1_EFAIL IAUDENC1_EFAIL |
#define | AUDENC1_EUNSUPPORTED IAUDENC1_EUNSUPPORTED |
#define | AUDENC1_ETIMEOUT VISA_ETIMEOUT |
#define | AUDENC1_FOREVER VISA_FOREVER |
#define | AUDENC1_VISATYPE "ti.sdo.ce.audio1.IAUDENC1" |
| The VISA type.
|
Typedefs |
typedef VISA_Handle | AUDENC1_Handle |
| Opaque handle to a AUDENC1 codec.
|
typedef IAUDENC1_Params | AUDENC1_Params |
typedef IAUDENC1_InArgs | AUDENC1_InArgs |
typedef IAUDENC1_OutArgs | AUDENC1_OutArgs |
typedef IAUDENC1_Cmd | AUDENC1_Cmd |
typedef IAUDENC1_DynamicParams | AUDENC1_DynamicParams |
typedef IAUDENC1_Status | AUDENC1_Status |
Functions |
Int32 | AUDENC1_control (AUDENC1_Handle handle, AUDENC1_Cmd id, AUDENC1_DynamicParams *params, AUDENC1_Status *status) |
| Execute the control() method in this instance of an audio encoder algorithm.
|
AUDENC1_Handle | AUDENC1_create (Engine_Handle e, String name, AUDENC1_Params *params) |
| Create an instance of an audio encoder algorithm.
|
Void | AUDENC1_delete (AUDENC1_Handle handle) |
| Delete the instance of an audio encoder algorithm.
|
Int32 | AUDENC1_process (AUDENC1_Handle handle, XDM1_BufDesc *inBufs, XDM1_BufDesc *outBufs, AUDENC1_InArgs *inArgs, AUDENC1_OutArgs *outArgs) |
| Execute the process() method in this instance of an audio encoder algorithm.
|
Int32 | AUDENC1_processAsync (AUDENC1_Handle handle, XDM1_BufDesc *inBufs, XDM1_BufDesc *outBufs, AUDENC1_InArgs *inArgs, AUDENC1_OutArgs *outArgs) |
| Perform asynchronous submission to this instance of an audio encoder algorithm.
|
Int32 | AUDENC1_processWait (AUDENC1_Handle handle, XDM1_BufDesc *inBufs, XDM1_BufDesc *outBufs, AUDENC1_InArgs *inArgs, AUDENC1_OutArgs *outArgs, UInt timeout) |
| Wait for a return message from a previous invocation of AUDENC1_processAsync() in this instance of an audio encoder algorithm.
|
Detailed Description
This is the audio encoder interface. Several of the data types in this API are specified by the XDM IAUDENC1 interface; please see the XDM documentation for those details.
Define Documentation
#define AUDENC1_EOK IAUDENC1_EOK |
#define AUDENC1_EFAIL IAUDENC1_EFAIL |
#define AUDENC1_EUNSUPPORTED IAUDENC1_EUNSUPPORTED |
#define AUDENC1_ETIMEOUT VISA_ETIMEOUT |
#define AUDENC1_FOREVER VISA_FOREVER |
Special value for timeout parameter indicating never timeout.
#define AUDENC1_VISATYPE "ti.sdo.ce.audio1.IAUDENC1" |
Typedef Documentation
Opaque handle to a AUDENC1 codec.
Defines the creation time parameters for all IAUDENC1 instance objects.
This structure defines the algorithm parameters that can be modified after creation via control() calls.
- See also:
- IAUDENC1_Fxns::control()
Function Documentation
Execute the control() method in this instance of an audio encoder algorithm.
- Parameters:
-
[in] | handle | Handle to a created audio encoder instance. |
[in] | id | Command id for XDM control operation. |
[in] | params | Runtime control parameters used for encoding. |
[out] | status | Status info upon completion of encode operation. |
- Precondition:
handle
is a valid (non-NULL) audio encoder handle and the audio encoder is in the created state.
- Return values:
-
- See also:
- AUDENC1_create()
-
AUDENC1_delete()
-
IAUDENC1_Fxns::control()
Create an instance of an audio encoder algorithm.
Instance handles must not be concurrently accessed by multiple threads; each thread must either obtain its own handle (via AUDENC1_create()) or explicitly serialize access to a shared handle.
- Parameters:
-
[in] | e | Handle to an opened engine. |
[in] | name | String identifier of the type of audio encoder. to create. |
[in] | params | Creation parameters. |
- Return values:
-
NULL | An error has occurred. |
non-NULL | The handle to the newly created audio encoder instance. |
- See also:
- Engine_open()
-
AUDENC1_delete()
Delete the instance of an audio encoder algorithm.
- Parameters:
-
[in] | handle | Handle to a created audio encoder instance. |
- Precondition:
handle
is a valid (non-NULL) handle which is in the created state.
- Postcondition:
- All resources allocated as part of the AUDENC1_create() operation (memory, DMA channels, etc.) are freed.
- See also:
- AUDENC1_create()
Perform asynchronous submission to this instance of an audio encoder algorithm.
- Parameters:
-
[in] | handle | Handle to a created audio encoder instance. |
[in] | inBufs | A buffer descriptor containing input buffers. |
[out] | outBufs | A buffer descriptor containing output buffers. |
[in] | inArgs | Input Arguments. |
[out] | outArgs | Output Arguments. |
- Precondition:
handle
is a valid (non-NULL) audio encoder handle and the audio encoder is in the created state.
- Return values:
-
- See also:
- AUDENC1_create()
-
AUDENC1_delete()
-
AUDENC1_control()
-
AUDENC1_process()
-
AUDENC1_processWait()
-
IAUDENC1_Fxns::process()
Wait for a return message from a previous invocation of AUDENC1_processAsync() in this instance of an audio encoder algorithm.
- Parameters:
-
[in] | handle | Handle to a created audio encoder instance. |
[in] | inBufs | A buffer descriptor containing input buffers. |
[out] | outBufs | A buffer descriptor containing output buffers. |
[in] | inArgs | Input Arguments. |
[out] | outArgs | Output Arguments. |
[in] | timeout | Amount of "time" to wait (from 0 -> AUDENC1_FOREVER) |
- Precondition:
handle
is a valid (non-NULL) audio encoder handle and the audio encoder is in the created state.
- Return values:
-
- See also:
- AUDENC1_create()
-
AUDENC1_delete()
-
AUDENC1_control()
-
AUDENC1_process()
-
AUDENC1_processAsync()