![]() |
![]() |
Defines the run time output arguments for all IVIDDEC instance objects. More...
#include <ividdec.h>
Data Fields | |
XDAS_Int32 | size |
XDAS_Int32 | extendedError |
XDAS_Int32 | bytesConsumed |
XDAS_Int32 | decodedFrameType |
XDAS_Int32 | outputID |
IVIDEO_BufDesc | displayBufs |
Defines the run time output arguments for all IVIDDEC instance objects.
size
parameter. size
field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
Extended error information.
Bytes consumed.
Decoded frame type. See IVIDEO_FrameType.
Output ID. Refer to comment IVIDDEC_InArgs::inputID.
The decoder fills this structure to denote the buffer pointers for current displayable frames. In case of sequences having I & P frames only, these values are identical to outBufs passed in process().