![]() |
![]() |
Defines the creation time parameters for all IVIDDEC2 instance objects. More...
#include <ividdec2.h>
Data Fields | |
XDAS_Int32 | size |
XDAS_Int32 | maxHeight |
XDAS_Int32 | maxWidth |
XDAS_Int32 | maxFrameRate |
XDAS_Int32 | maxBitRate |
XDAS_Int32 | dataEndianness |
XDAS_Int32 | forceChromaFormat |
Defines the creation time parameters for all IVIDDEC2 instance objects.
size
parameter. size
field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details. Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
Maximum video height in pixels.
Maximum video width in pixels.
Maximum frame rate in fps * 1000. For example, if max frame rate is 30 frames per second, set this field to 30000.
Maximum bit rate, bits per second. For example, if bit rate is 10 Mbps, set this field to 10000000
Endianness of output data.
Chroma formats.