![]() |
![]() |
Defines the run time output arguments for all ISPHENC1 instance objects. More...
#include <isphenc1.h>
Data Fields | |
XDAS_Int16 | size |
XDAS_Int16 | frameType |
XDAS_Int32 | extendedError |
Defines the run time output arguments for all ISPHENC1 instance objects.
size
parameter. size
field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
Encoder frame types.
Extended error information.