![]() |
![]() |
Defines the creation time parameters for all IIMGDEC1 instance objects. More...
#include <iimgdec1.h>
Data Fields | |
XDAS_Int32 | size |
XDAS_Int32 | maxHeight |
XDAS_Int32 | maxWidth |
XDAS_Int32 | maxScans |
XDAS_Int32 | dataEndianness |
XDAS_Int32 | forceChromaFormat |
Defines the creation time parameters for all IIMGDEC1 instance objects.
size
parameter. size
field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details. Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
Maximum image height.
Maximum image width.
Maximum number of scans.
Endianness of output data.
Chroma formats.