The Codec Engine Runtime init module. Provides system wide initialization of the Codec Engine Runtime.
#include <ti/sdo/ce/Engine.h>
Go to the source code of this file.
Defines | |
#define | CE_NULL_algs NULL |
#define | CE_DECLARE_TYPE(name, types) |
Macros for runtime configuration. These macros can be used to create a static table of algorithms. However, the preferred method of building engine and alg tables, is to use the run-time APIs, Engine_add() and Engine_addAlg(). | |
#define | CE_LOCAL_ALG(name, algName, ialgFxns, idma3Fxns, iresFxns, groupId, memType) |
Generates a structure containing data for a local algorithm. | |
#define | CE_LOCAL_ALG2(algName, ialgFxns, idma3Fxns, iresFxns, groupId, memType, types) |
Generates a structure containing data for a local algorithm. This macro takes a 'types' string as an argument to avoid having to use the CE_DECLARE_TYPES() macro call. | |
#define | CE_DECLARE_LOCAL_ALG(name, algName, ialgFxns, idma3Fxns, iresFxns, groupId, memType, types) |
Generates a static variable of type Engine_AlgDesc. It is used in this manner: | |
#define | CE_BEGIN_ALG_TABLE(name) static Engine_AlgDesc CE_##name##_algs[] = { |
Use this macro and the CE_END_ALG_TABLE() macro around CE_LOCAL_ALG() to generate an algorithm table for an engine. | |
#define | CE_END_ALG_TABLE(name) |
Use this macro after CE_BEGIN_ALG_TABLE() and CE_LOCAL_ALG() for generating an algorithm table for an engine. | |
#define | CE_ENGINE(algTab, engName, serverName, memMap, useExtLoader, heapId) |
Generates a structure containing data for an engine. | |
#define | CE_BEGIN_ENGINE_TABLE(name) |
Use this macro and the CE_END_ENGINE_TABLE() macro around CE_ENGINE() to generate an engine table for the application. | |
#define | CE_END_ENGINE_TABLE(name) |
Use this macro and the CE_BEGIN_ENGINE_TABLE() macro around CE_ENGINE() to generate an engine table for the application. | |
Functions | |
Void | CERuntime_exit (Void) |
Exit the Codec Engine Runtime. | |
Void | CERuntime_init (Void) |
Initialize the Codec Engine Runtime. |