Data Fields

IVIDANALYTICS_DynamicParams Struct Reference
[IVIDANALYTICS - XDM Beta Video Analytics Interface]

This structure defines the algorithm parameters that can be modified after creation via control() calls. More...

#include <ividanalytics.h>

Collaboration diagram for IVIDANALYTICS_DynamicParams:
Collaboration graph
[legend]

Data Fields

XDAS_Int32 size
IVIDANALYTICS_Gridgrid
XDM_Date date
IVIDANALYTICS_Rule rule

Detailed Description

This structure defines the algorithm parameters that can be modified after creation via control() calls.

Remarks:
It is not necessary that a given implementation support all dynamic parameters to be configurable at run time. If a particular algorithm does not support run-time updates to a parameter that the application is attempting to change at runtime, it may indicate this as an error.
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.
See also:
IVIDANALYTICS_Fxns::control()

Field Documentation

Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.

New overlay grid with analytics enable mask

Set the current time.

Rule associated with this command (if applicable).


The documentation for this struct was generated from the following file:
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2010, Texas Instruments Incorporated