Data Fields

ISPHENC_Fxns Struct Reference
[ISPHENC - XDM Speech Encoder Interface]

Defines all of the operations on ISPHENC objects. More...

#include <isphenc.h>

Collaboration diagram for ISPHENC_Fxns:
Collaboration graph
[legend]

Data Fields

IALG_Fxns ialg
XDAS_Int32(* process )(ISPHENC_Handle handle, XDM_BufDesc *inBufs, XDM_BufDesc *outBufs, ISPHENC_InArgs *inArgs, ISPHENC_OutArgs *outArgs)
 Basic speech/voice encoding call.
XDAS_Int32(* control )(ISPHENC_Handle handle, ISPHENC_Cmd id, ISPHENC_DynamicParams *params, ISPHENC_Status *status)
 Control behavior of an algorithm.

Detailed Description

Defines all of the operations on ISPHENC objects.


Field Documentation

XDAIS algorithm interface.

See also:
IALG_Fxns

Basic speech/voice encoding call.

Parameters:
[in]handleHandle to an algorithm instance.
[in]inBufsInput buffer descriptors.
[in,out]outBufsOutput buffer descriptors. The algorithm may modify the output buffer pointers.
[in]inArgsInput arguments. This is a required parameter.
[out]outArgsOuput results. This is a required parameter.
Remarks:
process() is a blocking call. When process() returns, the algorithm's processing is complete.
Precondition:
handle must be a valid algorithm instance handle.
inArgs must not be NULL, and must point to a valid ISPHENC_InArgs structure.
outArgs must not be NULL, and must point to a valid ISPHENC_OutArgs structure.
inBufs must not be NULL, and must point to a valid XDM_BufDesc structure.
inBufs.buf[0] must not be NULL, and must point to a valid buffer of data that is at least inBufs.bufSizes[0] bytes in length.
outBufs must not be NULL, and must point to a valid XDM_BufDesc structure.
outBufs.buf[0] must not be NULL, and must point to a valid buffer of data that is at least outBufs.bufSizes[0] bytes in length.
The buffers in inBufs and outBufs are physically contiguous and owned by the calling application.
Postcondition:
The algorithm must not modify the contents of inBufs. That is, the data and buffers pointed to by these parameters must be treated as read-only.
The buffers in inBufs and outBufs are owned by the calling application.
Return values:
IALG_EOKSuccess.
IALG_EFAILFailure. See ISPHENC_OutArgs::extendedError for more detailed further error conditions.

Control behavior of an algorithm.

Parameters:
[in]handleHandle to an algorithm instance.
[in]idCommand id. See XDM_CmdId.
[in]paramsDynamic parameters. This is a required parameter.
[out]statusOutput results. This is a required parameter.
Precondition:
handle must be a valid algorithm instance handle.
params must not be NULL, and must point to a valid ISPHENC_DynamicParams structure.
status must not be NULL, and must point to a valid ISPHENC_Status structure.
Postcondition:
The algorithm *must* not modify the contents of params. That is, the data pointed to by this parameter must be treated as read-only.
Return values:
IALG_EOKSuccess.
IALG_EFAILFailure. See ISPHENC_Status::extendedError for more detailed further error conditions.

The documentation for this struct was generated from the following file:
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2010, Texas Instruments Incorporated