Data Fields

IIMGENC_CodecClassConfig Struct Reference
[IMGENC - Image Encoder Interface]

Definition of IIMGENC codec class configurable parameters. More...

#include <imgenc.h>

Data Fields

Bool manageInBufsCache [16]
Bool manageOutBufsCache [16]

Detailed Description

Definition of IIMGENC codec class configurable parameters.

See also:
VISA_getCodecClassConfig()

Field Documentation


The documentation for this struct was generated from the following file:
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2010, Texas Instruments Incorporated